show the entry list
S7-300 CPU 31x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can user-defined web pages and standard web pages be updated automatically in STEP 7 (TIA Portal) V11?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) V11 as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How can time and date be acquired from a GPS signal?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
Where can I procure the GSD files for my S7-300 CPUs?
How do you configure time synchronization?
What is the startup behavior of an S7-300/400 CPU when you have configured an "empty" DP master system with "Startup when expected/actual configuration differ", but no slave is incorporated?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Connecting an S7-300 to a DP/PA-Link
Network transitions and links (DP) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you link the AS-i Slaves to an S7-300 CPU with integrated PROFINET interface using the IE/AS-i Link?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 via PROFIBUS using S7 Communication and incorporating an IE/PB Link gateway?
Where do you find sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway?
Where can you find sample programs and documentation for communication between a PC station and SIMATIC S7 using S7 communication and incorporating an IE/PB link gateway?
Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB
How do you configure a ring redundancy with FDC 157-0 DP/PA couplers and active field distributors (AFDs)?
Connecting an S7-300 to a DP/PA-Link
Which options do you have for accessing PROFIBUS devices from a PC behind an IWLAN/PB link PN IO or an IE/PB link PN IO?
How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5?(GSD-Tool)
Incorporating new LINK modules in PCS7 V4.02
Set-up restrictions when using universal modules
Reduced user data capacity when using the diagnostics
Reading the input data of a DP slave configured by a different DP master
How do you configure an S7-300 CPU or a CP342-5 as DP slave to an S7-400H as DP master using a Y-link?
Configuration of the I/O Data on DP/DP Coupler
Retrieve Diagnostics of the DP/AS-i Link 20E
Configuring I/O addresses with DP/AS-i Link 20E
What are the special features of input/output addressing with the DP/DP coupler?
Connecting an S7-300 to a DP/PA-Link
Part number:

 

QUESTION:
How can you link an S7-300 module as DP slave to a DP/PA-Link in the hardware configuration of STEP 7? 

ANSWER:  
The normal way of linking the above-mentioned modules from the PROFIBUS-DP catalog of the hardware configuration of STEP 7 to the DP master segment of the DP/PA-Link is not possible. Linking the S7-300 as slave to a DP/PA-Link is only possible via the GSD files. When handling CPU-I slaves via GSD file you must make sure as user that the I/O areas match each other.   First download the GSD files required for the above-mentioned modules onto your STEP 7 system.  If these GSD files are already incorporated in your hardware configuration, you can skip this step. The GSD files are available in the Internet in the Entry ID: 113652 "PROFIBUS GSD files : SIMATIC".   Via the menu item "Options > Install New GSD…" you can incorporate the GSD files in your hardware configuration. Please close your S7 station before doing this.

Fig. 1: Installation of the new GSD file of the catalog   

Open your hardware configuration again and configure the module IM157 (e.g. the DP/PA-Link with MLFB: 6ES7157-0AA81-0XA0). From the PROFIBUS DP catalog/subdirectory "DP/PA link" you can link this module directly to the segment of the redundant master system using drag-and-drop.

Fig. 2: Selecting the DP/PA link in the HW Config   

Specify a PROFIBUS address for the DP/PA-Link and select "Interface Module for PROFIBUS-DP" (see Fig. 3).

Fig. 3: Selecting the interface module in the HW Config   

You will then find the S7-300 modules in the PROFIBUS DP catalog under "Additional Field Devices" (see Fig. 4). 

Fig. 4: Selecting the S7-300 module   

Now use drag-and-drop to copy these modules to the master system. Make sure here that you select the right bus system (in Fig. 5: PROFIBUS (5)) and a PROFIBUS address.  If you use the GSD files available at the time, then the CPU 315-2 DP is incorporated as DPV0 slave.

Fig. 5: Configuration in the HW Configuration   

Now you still have to create the HW configuration for the CPU being operated as DP slave. In the case of a standard slave, you usually only have to set the DP address and the baud rate.   

Create an S7-300 station according to your HW configuration. 
Connect the DP interface to a bus. (You now have to select a bus other than the one on your DP/DP link, because you have already assigned the address for the DP slave here). 
Set the DP interface of the CPU to slave mode (double-click DP Interface > Operating Mode tab). Please make sure that the PG functions are not activated.

Fig. 6: Settings as DP slave   

Set the bus parameters for the bus. Use the same bus parameters as you have set on the secondary side of your DP/DP link. 
Load the configuration into the DP slave CPU.   

Keywords:  
Interface modules, I/O devices


 Entry ID:11645110   Date:2002-06-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour