show the entry list
S7-SCL -- Product information -- Information to predecessors
How can you query the status bit (BIE bit) in S7-SCL?
How can you debug multi-instances in S7-SCL?
How can you create the entries in the cross-reference list for FCs and FBs that are called in an SCL source?
Which bit data type conversion procedure has to be used for converting to the numerical data type "REAL"?
Why doesn't the compiler output any warning during the division of two integer values if the result has to be saved in the form of a real value?
Why do you get an error message when compiling with German mnemonics when the variables "a" and "e" are declared with the ARRAY data type?
Why is the following error message displayed when a REAL value is assigned: "Invalid data type"?
Why can't you load an OB (e.g. OB35) into the CPU?
While compiling the error "Internal error in move()" appears
How can you change the symbol name of a function in an S7-SCL source?
Why isn't the end of the comments recognized in the case of activated block comments?
What are the options for converting programs and sources from S7-SCL to ST (Structured Text) for the Rockwell Software in accordance with IEC 61131-3?
Optimization of the printouts of SCL-programs
Error message "Load PLC (294:23)" with SCL block and STRING_TO_CHAR" function
How can you optimize the runtime when accessing structures?
Different memory requirements depending on the used declaration types in SCL
How can you optimize the IF statement of a Boolean variable to shorten the cycle time?
Using program editor to view the STL code generated by SCL
Return value of STEP7 standard and system functions
Generating STL source from an SCL source
Difference between a symbolic variable and a local variable with the same syntax in SCL
Compiling SCL sources via SCL Makefile
Problems with allocating the L stack
Restrictions with the function "Continuous Monitoring"
How can you rewire block calls in the S7-SCL source?
Error message when calling an SFB
Type conflict when presetting DINT tags in the DB
Compiler error message: "Value excess in the constants"
Not possible to forward STRING variables
Apparent error function with command combination WORD_TO_BOOL(SHR/SHL(...))
All inputs in the SCL editor are underscored
Parameter SZL_HEADER of the SFC51 in SCL
Errors when compiling with SCL V5, version incompatibility with CFC V4
UNLINKED attribute in S7-SCL
Why does implicit data type conversion not take place under certain preconditions?
Order of creating variables in SCL 
In the Print Preview in S7-SCL only part of the code is displayed for multiple function blocks
How does processing work in S7-SCL if STEP 7 is in Chinese and a Chinese operating system (Windows XP) is installed?
Why does the compiler issue the message "Range of a standard function argument exceeded (15:16496)" with a statement with powers?
Why with S7-SCL programs written in an earlier version do you get a warning message in version V5.3 SP1?
SCL V5.1 SP3 block cannot be copied/found when compiling
Error when compiling: "Maximum number of testable components/instances is reached", debug information is not shown
Error when compiling: "Maximum number of testable components/instances is reached", debug information is not shown
Part number:
QUESTION:
Why, when compiling an SCL source with SCL Version V5.1+SP2, do I get the message "Maximum number of testable components/instances is reached" (1) and why, when I access the instance variables of an instance ">255" do I get no debug info shown (2)?  

ANSWER:
1) The message may be caused by the following:

  • The SCL source was created with SCL Version V5.0+SP3 and is now being compiled with SCL V5.1+SP2. In Version V5.0+SP3 this message did not appear after compiling.
  • If access to a certain data range is overwritten:  
    For example:
    The instruction:
    DB_Test.BST19:= 1; refers to the bit DB23.DBX512.6
    The instruction
    DB_Test.BST20:= 1; refers to the bit  DB23.DBX512.7

    If in DB23 you enter only the data range up to and including DBX512.6, you don't get any message. But as soon as you exceed this data range (from DB23.DBX512.7 on), the message appears.

Background:
Debug info can always only pass on 254 elements in the structure or interface of a function or data block. 
  

2.) Here again you have reached an internal system limit that can't be exceeded.  

Remedy:
Include the function block to be called as a statistical variable in the variables declaration of that block. In this function block call more function blocks, but not with their own instance data blocks. In this way you will concentrate the instance data in one instance data block, which means you can utilize the available number of data blocks more satisfactorily. Call the blocks for the multi-instance in question as a global instance for test purposes. After that the debug info can be generated. Once the function has been tested, the block with the planned multi-instance calls can be properly recompiled (but this time with no debug info).   Instead of using a command sequence such as:

    Instance1(...);

     x := Instance1.y;

you should use the instructions

    FB1.DB257(...);

     x:= DB257.y;

Extract from the Readme file for SCL Version V5.1 + SP 2 (Point 1 Service Pack 2): Service Pack 2 (S7-SCL K5.1.2) contains the following corrections for S7-SCL V5.1 + SP1. If structures have more than 254 components, the first 254 of them can now be monitored again for testing. The other components are not shown.  

Keywords:  
Debug info, Compilation error, Compiler message, Compiler, Development environment, Debugger.   

 Entry ID:10882543   Date:2002-05-02 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour