show the entry list
AS-Interface master -- Product information -- System description
3RK AS-i General: Determination of I/O addresses of an AS-i slave
Meaning of I/O code and ID, ID1, ID2 code in conjunction with AS-Interface modules
What is the significance of the IP protection classes IP65, IP66, IP67?
Which software do you need for the C7-621 module (with integrated AS interface master)?
AS-Interface Slaves -- Hardware aufbauen und parametrieren -- Geräte konfigurieren
3RK AS-i General: Determination of I/O addresses of an AS-i slave
How are Asi-A slaves and Asi-B slaves to be addressed with the CP 343-2?
How must an AS-Interface 16 I module be addressed?
What Bit addresses are used in 2 I / 2 O AS-Interface Modules?
3RK AS-i General: Determination of I/O addresses of an AS-i slave
Part number:

QUESTION:

How can you determine the I/O addresses of an AS-i slave regardless of the AS-i Master used when the initial address of the binary I/O area is known?

 

 

ANSWER:

When using an AS-i Master in automation systems, you must define an I/O address area for each AS-i Master in the hardware configuration. This results in a fixed binary I/O address area each of four input bits and four output bits for every possible standard slave (A slave) depending on the its slave address (1 to 31). In order to determine the address assignment of your AS-i slave relatively quickly during continued configuration, you can use the Excel table in the "Adressbelegung_ASI.zip" file below (address assignment_ASI). You just have to enter the initial address of the I/O area of the AS-i Master in Field 4 of the table. After transfer, the resulting address area of all possible AS-i slaves is displayed.
Download the "Adressbelegung_ASI.zip" file into a directory of your choice and then extract it. You can now use the Excel table.

 

 Adressbelegung_ASI.zip (5 KB) ( 5 KB )

 

Keywords: Address assignment, Address dependency

 

 Entry ID:10786938   Date:2012-03-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour