show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
TeleService/TS/PC Adapter -- Setting up and parameterizing hardware -- Configuring devices
Which settings and parameters are required to create a gateway from GSM to ISDN with TeleService S7?
How do you parameterize the TS Adapter II / IE modems for Australia and New Zealand?
TeleService with ET200S (IM151-CPU) and TS Adapter
How can the TS Adapter II be parameterized for the SINAUT GSM modem MD720-3?
How is the TS Adapter IE parameterized for an EDI connection with the product PCAnywhere?
What should you watch out for when parameterizing the initialization string for a modem with TeleService?
How do you commission a GSM wireless modem of the type M20 Terminal with TeleService S7 V5.x?
How are remote monitoring and control performed with TeleService IE?
What are the options for using the TS Adapter IE as standard router?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you set the local modem after installing TeleService V6.1?
Check list for implementing a PC adapter
How do you commission the TS adapter V5.x with the GSM modules TC35 terminal and TC35i terminal?
Call-back feature of the TS adapter v.5.x
Connecting to the Network via Auxiliary System
TeleService with ET200S (IM151-CPU) and TS Adapter
Part number:

QUESTION:
How do I run TeleService with the ET200S (IM151-CPU)?

ANSWER:
You want to set up a remote link to an ET200S (IM151-CPU).

The following components are available for running TeleService with the ET200S (IM151-CPU):

  • SIMATIC TeleService as Options Package for STEP 7
  • TS Adapter



TeleService enables the follow operating modes:

  1. Teleservice
  2. PLC - PG/PC remote link
  3. PLC – PLC remote link




1. Teleservice

In this operating mode a connection is set up from the PG/PC to the ET200S CPU. The ET200S is server. This also permits unrestricted operation with a passive interface on the ET200S.

Here the local PG/PC sets up a remote connection via modem to the remote TS Adapter itself, then an S7 connection to the remote CPU. Via the connections that have been set up you can run the STEP 7 services such as Download/Upload, Status/Control, Online Diagnostics etc. on the remote CPU.



Figure 1: Teleservice

2. PLC - PG/PC remote link

This type of link is not possible in an ET200S CPU with passive DP interface for the following reasons:

In this operating mode an S7 connection is set up via the function block "PG_DIAL" from the PLC to the local TS Adapter. The function block "PG_DIAL" is supplied with the TeleService software and integrated into the installed STEP 7 package. The "PG_DIAL" FB internally calls the blocks of the S7 basic communication: X_SEND and X_GET. The TS Adapter itself then sets up a remote connection to the remote PG/PC via the connected modem. In this connection, an application (created with PRODAVE MPI) plays the relevant partner. In this case then the CPU must take the initiative to set up a connection. This is only possible if the interface of the CPU is active and has MPI properties (S7 basic communication supported with X blocks).



Figure 2: PLC-PG remote link

3. PLC – PLC remote link

This link is for the CPU-CPU communications via WAN. At least one partner must take the initiative to set up the connection (initiator) and for this the communications interface of this partner must be active and the blocks of the S7 basic communication available (X_PUT, X_SEND, X_GET, X_ABORT). For the other partner it is sufficient to have the server functionality, this is then also possible with a passive interface.

An S7 connection to the local TS Adapter is set up via the function block "PLC_DIAL" in the local CPU. The function block "PLC_DIAL" is supplied with the TeleService software and integrated into the installed STEP 7 package. The "PLC_DIAL" FB supplies the selection information to the local TS Adapter and then the TS Adapter sets up a remote connection to the remote TS Adapter via the connected modem. During data transfer, the remote TS Adapter behaves like a "transparent router". It sets up an S7 connection to the remote CPU and with the operating firmware of the remote CPU it executes the X_GET and X_PUT tasks without there being a need for a user program for this functionality on the remote CPU.

The ET200S CPU has a passive interface and thus supports a PLC-PLC remote link as server, though only for the system functions X_PUT and/or X_GET in the initiator (local CPU). The PROFIBUS interface of the ET200S can then be compared with an MPI interface (PB address = MPI address). The ET200S must be connected to the same PROFIBUS segment as the TS Adapter. When parameterizing the TS Adapter, you must set the PROFIBUS profile that corresponds to the ET200 CPU.

Figure 3: PLC-PLC remote link

Keywords:
Teleservice

 Entry ID:10429562   Date:2002-03-12 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour