show the entry list
ProTool -- Configuring and programming communication -- Configuring communication to S7
Settings in "Status/Force" when using a WinAC MP
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
Connecting a panel to a S7 300/400 controller
Connection settings for a communication between ProTool/Pro and WinAC
How can you increase the performance of HMI devices?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
ProTool/ProRT and S7-200 with PC/PPI-Cable
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Coupling between ProTool/Pro and WinAC
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
ProTool RT -- Configuring and programming communication -- Configuring communication to S7
PPI connection of ProTool/Pro and S7-200
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a panel to a S7 300/400 controller
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
ProTool/ProRT and S7-200 with PC/PPI-Cable
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
Coupling between ProTool/Pro and WinAC
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
What should you watch out for with the PPI/MPI/DP interfaces if you want to use the CP 5711 with a SIMATIC S7-200?
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
PPI connection of ProTool/Pro and S7-200
Part number:

QUESTION:
Can you connect the runtime version of ProTool/Pro with an S7-200 via PPI?

ANSWER:
ProTool V5.2 / SP 1 and lower:
In the description you have read that it is possible to connect the runtime version of ProTool/Pro with an S7-200 via PPI. But a PC/PPI cable is not sufficient for this. You need the CPs CP5411, CP5511, CP5611 or MPI on-board. Also, when using the PPI protocol, you should note that only one S7-200 controller can be addressed. With MPI you can use several controllers. 

ProTool V5.2 / SP 2 and higher:
The following PC/PPI cable is released as a pure point-to-point interface between a ProTool/Pro Runtime (V5.2 / SP2 and higher) and a SIMATIC S7-200:

  • MLFB 6ES7 901-3BF20-0XA0

The necessary drivers are installed automatically with ProTool/Pro Runtime V5.2 / SP2. The drivers are released for Windows 95/98.

Keywords:
Communications

 Entry ID:1022975   Date:2001-09-04