show the entry list
WinCC SIMATIC Logon / AUA -- Product information -- Information on SIMATIC Logon / Advanced User Administrator
Using a chip card reader, how can a default user be logged on automatically while the chip card is pulled through?
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of WinCC comply with FDA regulations?
How can you configure a chip card with SIMATIC Logon, with which you can log onto each local computer?
Why isn't the group selection dialog displayed any longer in WinCC V6.2 and higher?
How can you use the "GetSignature" function as of SIMATIC Logon V1.4?
What is the standard password of the user "Administrator" in the WinCC User Administrator?
Why isn't the user currently logged on shown at Runtime?
How can you replace the Windows on-screen keyboard of SIMATIC Logon (from V1.4) with the ProTool keyboard so as not to reach the operating system during Runtime?
How can you verify a logged on user at runtime when using SIMATIC Logon (as from V1.3)?
How can you verify a logged on user at runtime when using SIMATIC Logon up to version V1.2 SP1?
How do you call the SIMATIC Logon dialog box by means of C-Script?
The WinCC Login Box appears instead of the Logon Box in WinCC Runtime.
OS - WinCC -- Creating HMI configurations -- Configuring User Administrator
How in PCS 7 can you prevent a user with "Monitor" rights from acknowledging messages?
How do user rights (authorizations) work in SIMATIC PCS 7 V7.1?
What is the standard password of the user "Administrator" in the WinCC User Administrator?
How can you set up auto logon for SIMATIC IPCs?
PCS 7 V6.0 / WinCC V6.0 operator right during Remote-access to Server
Executing actions depending on authorization level
Which setting options do I have when logging on with the chip-card reader (PCS 7 V4.x / V5.x)?
There are too many authorization levels in the User Administrator
Why doesn't the area-specific authorization work although it has been set in the User Administrator?
How can you realize login via chip card in PCS 7 with SIMATIC Logon?
What is the standard password of the user "Administrator" in the WinCC User Administrator?
Part number:

Description
With a new project the user "Administrator" is always created in the WinCC User Administrator. The password is Administrator.

Note
Please replace the default password for the user Administrator with your own password.

 Entry ID:10087466   Date:2009-12-28 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour