show the entry list
ASIsafe -- Hardware aufbauen und parametrieren -- Geräte konfigurieren
3RK1 ASIsafe: Recognition of short-time errors (safety component releases for a short time)
3RK1105 AS-i Safety monitor: Suppressing short-term faults with a time delay
3RK1 ASIsafe: Connecting two AS-Interface bus systems which contain Safety at Work
3RK1105 AS-i Safety monitor: Suppressing short-term faults with a time delay
Part number:

QUESTION:

Can short-term faults on the Safety at Work bus be suppressed with a time delay (i.e. does the monitor go into error mode if the release is shorter than the time delay, or does it remain switched on)?

 

 

ANSWER:

In this case, it depends on the type of error. Incorrect transferred Code sequences can not be suppressed generally. Short-term contact openings (for example because of vibration) may be suppressed by a time function element (switch-off delay), but results in a delayed switch-off also in the error-free operation. This switch-off delay would neither detect the relevant and safe AS-i-Slave in case of a failure of the AS-i-Bus (during the waiting time).
Those measures extend the total response time and are normally incompatible with the safety requirement.

Therefore, we recommend to remove the cause and not to evade the reaction.

 

 Entry ID:10052275   Date:2012-03-19 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour