show the entry list
ASIsafe -- Produktinformationen -- Systembeschreibung
3RK1105 AS-i Safety monitor: Behavior when the bus or the connected devices show faults
3RK1105 AS-i Safety monitor: Purpose of terminal FE (Functional Earthing)
3RK1105 AS-i safety monitor: Does the ASi-monitor switch off if the CPU starts up with CP343-2 ?
DP/AS-i F-Link: The inputs of the ASIsafe slaves which are connected via DP/AS-i F-Link are zero in the failsafe program
3RK1105 AS-i Safety monitor: Behavior when the bus or the connected devices show faults
Part number:

QUESTION:

Is it true that the 3RK1105 AS-i Safety monitor detects external faults, e.g. EMERGENCY-STOP button defective, repeater or 30 V DC power supply unit faulty, AS-Interface Bus faulty / capped and contacts from the Safety Monitor open?

 

 

ANSWER:

If EMERGENCY-STOP buttons (F adapters), repeaters, 30 V DC power supply units or AS-Interface Bus are defective or faulty, the contacts of the 3RK1105 AS-i Safety monitor open.

 

 Entry ID:10000325   Date:2012-03-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour