show the entry list
PROFIBUS general -- Product information -- System description
Which PROFIBUS connectors can you use in Zone 1 or 2?
Start-up characteristics of DP configuration after power supply OFF/ON
Parameter DP Master System ID
Failure of a master in a multimaster system
PRB checker with the Windows language setting German (Switzerland) 
Sporadic bus error with SIMATIC OPs on distributed I/O under S5 masters
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
Using S7 Communication, MPI, FDL or FMS on a PROFIBUS master system with Power Rail Booster
Changing from EN50170 to DPV1
Which products can you use with an RS 485-IS segment?
What options exist for using the BT200 tester on the PROFIBUS?
Which terminology do you use for cyclic PROFIdrive communication?
Which manuals are available to download from Industry Online Support regarding the diagnostic repeater and the RS 485 repeater?
Communication between two IM151 CPUs
How can you print on just one page the network topology determined via the Diagnostics Repeater?
Transferring the registration key to another PC/PG
Failure of a master in a multimaster system
Part number:

QUESTION:
If one master fails in my multimaster system, are the other systems still able to communicate?

ANSWER:
In your network there are multiple masters that each have access to multiple slaves. If one master fails, e.g. through power failure or another technical defect, then the following must be noted:
If the failure of one master in a multimaster system is due to a hardware fault, then under circumstances the complete network can be put out of action through a short-circuit on the bus line. In this case the fault must be cleared and the defective master removed from the network. If the failure of the master has no direct effect on the electrical properties (e.g. CP in STOP mode or power failure of the complete station), then the network can continue working.

If the master concerned is the last bus user in the bus network, then the following must be noted for PROFIBUS/MPI:
The open PROFIBUS line end must always have an active terminating element, i.e. one to which power is applied. This prevents reflections (noise or interference signals through periodic and/or random deviations) on the bus line. This is the only way for the other stations to be able to continue with unimpaired data communications. You can use the terminator that is included in the PROFIBUS connectors, but this has the disadvantage that if the complete station fails (e.g. through power supply failure), the network terminator is also lost. Then your complete network fails. It is better to use an external terminator (MLFB: 6ES7972-0DA00-0AA0), that is independent of the power supply of the automation systems.

Note:
You do not need a terminator for Industrial Ethernet.

If the failed master does not cause a bus short-circuit, then it does not need to be isolated from the bus. The communication of the intact master stations with their slaves is not affected.
The other masters can continue to have data communications with their slaves. The total cycle time is even shortened by the bus access time of the failed master.

Keywords:
Network nodes


 Entry ID:7764826   Date:2001-07-10 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour