show the entry list
PROFIBUS general -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
Which options are available for configuring the ET 200 stations?
Configuration of the alarm mode in STEP 7 for the diagnostics repeater (6ES7 972-0AB01-0XA0)
Correction to bus time calculations
Basic knowledge for configuring PROFIBUS-DP networks
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
Cyclic program processing only once all the DP stations have signaled that they are finished
Which parameters must be taken into account when planning an electrical network?
How can you calculate the bus cycle time on the PROFIBUS DP with STEP 7?
Basic knowledge for configuring PROFIBUS-DP networks
Part number:

QUESTION:
With what and how do I configure the hardware for a PROFIBUS-DP master/slave communication?

ANSWER:
Basically you have two options for configuring a PROFIBUS-DP master-slave communication. For this you can use either COM PROFIBUS or STEP 7. . Both configuration tools provide a wide range of devices for DP masters and slaves. If your slave is not available, then you can add this slave to the hardware catalog of each tool via a GSD file. You can procure the GSD files from the Internet pages of Customer Support under
"Automation Systems > SIMATIC Distributed I/O > GSD Files" in the "Download" tab.

Note:
PROFIBUS-DP master devices cannot be added subsequently in this way. For this you always have to install the latest version of STEP 7 or COM PROFIBUS.

Further information can be obtained from the manual "Configuring Hardware and Communication Connections with STEP 7 V5.3" under Entry-ID: 18652631. It lists important notes for the configuration of PROFIBUS-DP Networks. Moreover,you get detailed information on your DP slave from internet pages of the Customer Support under:
"Automation systems > SIMATIC Distributed Periphery  > /your DP-Slave/" in tab "manuals/BA".

Keywords:
Hardware configuration, System configuration


 Entry ID:7745186   Date:2004-05-19 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour