show the entry list
Product announcement, SIJECT 15 and 16
Part number:
Summary Internet document



SIJECT 15/16 is a compact control system for injection molding machines and extrusion systems. SIJECT 15/16 comprises two components, the Operator Panel (OP) and a compact interface (CI Board).

SIJECT 15 has been developed for the Asian and Chinese markets and has a compact interface with a soft PLC (IEC compatible).

SIJECT 16 has been developed for the world market and has a CI board with a S7-300 PLC.

Order Nos.

SIJECT16 DP Int. System	6AT1131-6CE20-0XA0

SIJECT16 Int. system 6AT1131-6CD20-0XA0

CI 16 DP Int. module 6AT1131-6DE20-0AA0

CI 16 Int. module 6AT1131-6DD20-0AA0

OP 15 Operator Panel 6AT1131-5BB20-0XA0

The following components can be ordered through SNC, Nanjing:

Name

Part No. (SNC number)

Comments

SIJECT15

SNC_185 010901 600

System

SIJECT15+

SNC_185 010901 500

System

CI15

SNC_185 012900 500

Module

CI15+

SNC_185 012900 400

Module



Internet document Summary


Thanks to its light, compact operator panels and the upright format, SIJECT 15/16 can be adapted to almost any environment.

Furthermore, the control functions are separately accommodated in a compact interface and can be connected to the operator panel using a cable. SIJECT is also protected against possible interference (noise, disturbances) as a result of the rugged metal housing. The operator panel and control unit can be easily installed without requiring any tools; I/O signals are connected via a standard connector.

CI15 only has digital inputs; CI15+ can support an additional two analog inputs (linear scale). CI15 and also CI15+ use a soft PLC (Siject Project Tool). Various programming versions are possible, including the programming language "ladder diagram". The device can be programmed using any PC with RS232 interface.

The compact SIJECT 16 control

Design, SIJECT 16: OP 15 and compact interface CI 16 (with integrated CPU 314)

Design, SIJECT 16 DP: OP 15 and compact interface CI 16 DP (with integrated CPU 315 DP)

SIJECT 16 is orientated to a higher market segment. SIJECT 16 can be combined with other OPs via the MPI interface. It can be expanded using all of the standard S7-300 I/O modules via the integrated P bus - interface and an interface module (IM 361). CI16DP has a PROFIBUS interface and can therefore be integrated into distributed control structures.
A SIMATIC S7-314 can be used as hardware PLC for CI16 - SIMATIC S7-315 for CI16DP. This means that SIJECT 16 can be programmed, parameterized and configured using the SIMATIC Manager and standard - STEP 7, which are known worldwide.

SIJECT15 was especially designed for the Chinese/Asian markets. This is the reason that all outputs switch w.r.t. a negative potential (n circuit configuration). On the other hand, SIJECT16 will be marketed globally which is why it is marketed switching w.r.t. a positive potential (P circuit configuration) (international version).



 Entry ID:7672810   Date:2001-06-19 
I regard this article....as helpfulas not helpful                                 
related links
New version of the "SIJECT Q ...
SIJECT 16 / 16 DP The perfect so ...
The version 08-2006 of the " ...
SIJECT 15/16. New Start-Up, SW ve ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour