| Operating system |
Procedure |
| Windows NT |
- In the Control Panel you select "Network", then select "Network card" and click the "Add" button.
- From the list displayed you select "MS Loopback Adapter" and install it.
You need the Windows NT CD-ROM for this procedure. |
| Windows 2000 |
Detailed instructions are available from Microsoft at this link: http://support.microsoft.com/kb/236869 |
| Windows XP, Windows Server 2003 |
Detailed instructions are available from Microsoft at this link: http://support.microsoft.com/kb/839013 |
| Windows Vista |
Select the Classic view and then proceed as for Windows XP. |
| Windows Server 2008 |
Select the Classic view and then proceed as for Windows XP. |
| Windows 7 |
Select "Start > Control Panel > Device Manager > Network Adapters". Select "Action > Add Legacy Hardware" and then proceed as for Windows XP. |