DESCRIPTION:
Update3 for WinCC flexible 2008 Service Pack 3 is now available.
Installation requirement:
WinCC flexible 2008 Service Pack 3 Micro
WinCC flexible 2008 Service Pack 3 Compact
WinCC flexible 2008 Service Pack 3 Standard
WinCC flexible 2008 Service Pack 3 Advanced
WinCC flexible 2008 Service Pack 3 ASIA Standard
WinCC flexible 2008 Service Pack 3 ASIA Advanced
WinCC flexible 2008 Service Pack 3 CHINA
WinCC flexible 2008 Service Pack 3 Runtime
Information on Update3 The Update must be installed on the Engineering System as well as on the Runtime Systems. The Operating System of the HMI devices also has to be upgraded by an operating system update (image update). The following Readme / Function description contains important information.
Liesmich ( 119 KB ) Readme ( 118 KB )
If you have problems in the use of the Update, please take contact with the Customer Support.
Update3 Download
Update3 includes also all previous Updates.
Please note the file size.