show the entry list
Technology CPUs: "Kinematics Simulation Center" - Connecting the Simulation Software to a Technology CPU Interface
Part number:

Task
Using the Technology CPU, you have or create an application in which you use the kinematic transformation via a path object in the Technology CPU and wish to monitor your programmed motions of the kinematics or the kinematic axes.

Solution  
The "Kinematics Simulation Center" (KSC) provides you with the option to represent the motions of the kinematic configured at a path object in the Technology CPU in an animated form on a Windows PC. For this purpose, the "Kinematics Simulation Center" (KSC) includes all kinematics available for a path object in the Technology CPU.

"Kinematics Simulation Center" (KSC) or Windows PC are connected to the Technology CPU via Ethernet using a "CP 343-1 Lean" or "CP 343-1" communication processor attached to the Technology CPU.

The application description on hand contains all information for using and connecting the "Kinematics Simulation Center" (KSC) to the Technology CPU. The driver blocks required for the Technology CPU are offered as a download. Configuration files for the basic configuration of the "Kinematics Simulation Center" (KSC) and an example project for immediate usage of the "Kinematics Simulation Center" (KSC) are available.

Downloads
Contents of the downloads

Download

Documentation 
Connecting the "Kinematics Simulation Center" simulation software to a Technology CPU
58260820_CPU31xT_Kinematics_Simulation_Center_DOKU_V11_en.pdf ( 8268 KB )
S7-Code 
Driver block for connecting the Technology CPU to the "Kinematics Simulation Center" (KSC).
58260820_CPU31xT_Kinematics_Simulation_Center_CODE_KSC-S7-Driver.zip ( 61 KB )
Link
The "Kinematics Simulation Center" (KSC) software can be downloaded under entry ID:
Entry ID 54759648
Configuration files
Configuration files for the "Kinematics Simulation Center" (KSC) for basic configuration of the simulation software suitable for the description illustrated in the documentation.
58260820_CPU31xT_Kinematics_Simulation_Center_CODE_KSC_Settings.zip ( 4 KB )
S7-Code 
Example project for the Technology CPU with connection to the "Kinematics Simulation Center" (KSC).
The example project is based on FAQ "How can a simple palletizer be realized with a Technology CPU and the FB 488 "MC_MovePath"?"
The documentation on function and operation of the example project is available at entry ID 48206063
58260820_CPU31xT_Kinematics_Simulation_Center_CODE_KSC_Example.zip ( 7814 KB )

Notes on the use of a communication processor
The "CP 343-1 Lean" and "CP 343-1" communication processors can be used together with the "Kinematics Simulation Center" (KSC) only from a certain firmware version on.

The following must apply for the firmware:
 
CP 343-1 Lean 6GK7 343-1CX10-0XE0 as of firmware V2.1
CP 343-1 6GK7 343-1EX21-0XE0 as of firmware V1.0.17
6GK7 343-1EX30-0XE0 as of firmware V2.0.16

Background
For the connection diagnostic, the FC 10 "AG_CNTRL" block with commands CMD=1 and CMD=2, whose function depends of the used firmware of the communication processor, is used in the driver block of the "Kinematics Simulation Center" (KSC).
The firmware version required for the communication processor can be determined in entry ID 33414377.
The usable communication processors, which support the FC 10 "AG_CNTRL" function, are listed under the following entry ID 16767769.

Note on security
Caution
The functions and solutions described in this entry are mainly limited to the realization of the automation task. In addition, please note that suitable security measures in compliance with the applicable Industrial Security standards must be taken if your system is interconnected with other parts of the plant, the company network or the Internet. More information can be found under entry ID 50203404.

Last modification
February 2012: First issue.
May 2012: Documentation adapted for internet publishing

Filter criteria:
Hardware platform: SIMATIC S7-300/S7-400
Software: S7-Technology
Entry contents: Function blocks/tools
 Entry ID:58260820   Date:2012-06-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
Contact
Support Request
Contacts worldwide
Technical Forum
QuickLinks
Compatibility tool 
Performance Data 
Micro Automation Sets
Help
Online Help
Guided Tour