show the entry list
S7-300 CPU 31x -- Configuring and programming communication -- Configuring PROFINETinterfaces
PROFINET - An Overview of the Most Important Documents and Links
In the user program, how do you read out the Link State of the PROFINET interface of a S7-300 CPU?
Which settings do you have to make in the TIA Portal to read out messages and status information over the CPU's web server and display them in the web browser?
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
How do you reset the IP address and device name of an I device?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you activate the "Prioritized OCM communication" function to improve the OP communication performance?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which CPU can you operate as a PROFINET I device?
What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the Internet?
In the user program of an S7-300 or S7-400 CPU with integrated PN interface, how can you read out the current topology of the PROFINET IO system connected?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
Which settings are required to access the web server of the CPU via a PC with a second network card even though a proxy server is set?
Can you implement an S7 317-2 PN/DP CPU instead of an S7 315-2 PN/DP CPU configured in iMap?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
What can you do when communication errors occur sporadically with a PROFINET interface of the S7 300 CPU 31x-2 PN/DP?
From which library should you take the communications FBs?
What are the commonalities and differences between configured communication connections and the open Ethernet communication?
What are the differences when assigning the MAC address?
S7-400 CPU 41x -- Configuring and programming communication -- Configuring the PROFINET interface
Which settings do you have to make in the TIA Portal to read out messages and status information over the CPU's web server and display them in the web browser?
Why is the "Certificate error" message shown in the address line when downloading the web page of an S7-300/400/1200 CPU over "https://..."?
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which CPU can you operate as a PROFINET I device?
What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the Internet?
In the user program of an S7-300 or S7-400 CPU with integrated PN interface, how can you read out the current topology of the PROFINET IO system connected?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Which settings are required to access the web server of the CPU via a PC with a second network card even though a proxy server is set?
What differences are there when configuring S7 connections?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Why is the menu item for starting S7-PCT in STEP 7 disabled in some IO Link master modules?
How can you group together the address area of the ET 200S in STEP 7 (TIA Portal) using the "Pack Addresses" function?
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
ET 200pro -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
Which options are available for configuring the ET 200 stations?
How do you set the addresses for the fail-safe I/O modules ET 200S and ET 200pro?
WinAC RTX F -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
How can you enable the Autostart function in WinLC so that WinAC starts automatically when the PC starts up?
Information about the topic of "Initializing and parameterizing modules"
Which PCI slots in the SIMATIC PCs have exclusive use of the interrupt - i.e. don't share it with other PCI devices?
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Why is there no entry with the current firmware version for my module in the STEP 7 hardware catalog?
What should you watch out for when a MAC address is entered for the PROFINET interface or GBIT interface in the configuration of the Industrial Ethernet CP343-1/CP443-1?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Which Industrial Ethernet CPs support the DHCP Option 12 (Host Name) and how do you configure the DHCP Option 12?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
How do you disable the "Link Layer Discovery Protocol" function at the ports of an IE CP of S7-300 or S7-400?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Changing the configuration data of users for CP 343-1 IT and CP 443-1 IT
Loading the configuration via LAN into the IE-CP in "STOP" mode
Special points when setting the LAN medium for Industrial Ethernet CPs
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Rejected diagnostics connection via TCP/IP protocol after changing the MAC address
Establishing an online connection to an S7-300/S7-400 CPU through several Ethernet interfaces
What should you pay attention to when formatting the file system in the S7-300 and S7-400 Industrial Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
What is the meaning of the configuration option "Activate Web server" with CP443-1 EX20?
Why with CP443-1 Advanced is a different firmware version than the module displayed in the C-PLUG info text in the NCM S7 Diagnostics?
Which options are available for assigning the PROFINET IO controller a new IP address?
How can you configure an S7 CP during runtime?
How do you disable the S7 routing functions?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What should you watch out for when using the function block FB55 "IP_CONFIG" to configure an Industrial Ethernet CP?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
Why can't my SIMATIC S7-300 Ethernet CP run as many S7 communication connections as specified?
How does connection multiplexing work and how do you configure it for SIMATIC S7-300 Ethernet CPs?
SINUMERIK 840D -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
How to save GUD variables and activate them later
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Part number:

Description
Depending on the module and interface through which the connection with the FB65 "TCON" for open communication over Industrial Ethernet is established, you parameterize the "local_device_id" accordingly.

The "local_device_id" for the S7-300 and S7-400 CPUs as well as for the IM151-8 PN/DP CPU and IM154-8 CPU is in the Hardware Configuration (STEP 7 V5.5) or in the Device View of the hardware and network editor (STEP 7 Professional V11). The slot identification for a module's PROFINET interface contains the "local_device_id".

Example for STEP 7 V5.5
The slot identification for the PROFINET interface on a CPU319-3 PN/DP is "X3", in other words you parameterize the "local_device_id" = B#16#03 for open communication through the integrated PROFINET interface on a CPU319-3 PN/DP.


Fig. 01

Example for STEP 7 Professional V11
The slot identification for the PROFINET interface on a CPU319-3 PN/DP is "2 X3", in other words you parameterize the "local_device_id" = B#16#03 for open communication through the integrated PROFINET interface on a CPU319-3 PN/DP.


Fig. 02

Note
The slot identification for the PROFINET interface on an S7-300 CPU, S7-400 CPU, IM151-8 PN/DP CPU or IM154-8 CPU is also printed on the module.

Overview
The overview below contains the "local_device_ids" which are to be parameterized for open communication by means of WinAC RTX and S7-400 Industrial Ethernet CP. The "local_device_id" of the WinAC RTX depends on the interface slot of the Industrial Ethernet interface.
 
local_device_id Description
B#16#00 Communication over Industrial Ethernet CP of the S7-400 (only with ISO-on-TCP, that means connection_type = B#16#12).

Note
Entry ID 15368142 contains information about which S7-400 series Industrial Ethernet CPs support open communication services using T blocks.

B#16#01 Communication through the Industrial Ethernet interface at interface slot 1 (IF1) with WinAC RTX.
B#16#06 Communication through the Industrial Ethernet interface at interface slot 2 (IF2) with WinAC RTX.
B#16#0B Communication through the Industrial Ethernet interface at interface slot 3 (IF3) with WinAC RTX.
B#16#0F Communication through the Industrial Ethernet interface at interface slot 4 (IF4) with WinAC RTX.

The overview below shows the "local_device_id" designations that you parameterize for open communication through the integrated PROFINET interface of an S7-300 CPU, S7-400 CPU, IM151-8 PN/DP CPU or IM154-8 CPU.
 
local_device_id Description
B#16#01 Communication through the integrated PROFINET interface of the IM151-8 PN/DP CPU.
B#16#02 Communication through the integrated PROFINET interface of the CPU31x-2 PN/DP, CPU314C-2 PN/DP and IM154-8 CPU.
B#16#03 Communication through the integrated PROFINET interface of the CPU319-3 PN/DP, CPU315T-3 PN/DP, CPU317T-3 PN/DP, CPU317TF-3PN/DP.
B#16#04 Communication through SINUMERIK NCU7x0.2 PN with CPU319-3 PN/DP and SINUMERIK NCU7x0.3PN with CPU317-2 PN/DP
B#16#05 Communication through the integrated PROFINET interface of the CPU412-2 PN, CPU414-3 PN/DP, CPU416-3 PN/DP and CPU41x-5H PN/DP (Rack 0).
B#16#15 Communication through the integrated PROFINET interface of the CPU 41x-5H PN/DP (Rack 1).

 Entry ID:51339682   Date:2013-08-30 
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
Themen
Help
Online Help
Guided Tour