show the entry list
STEP 7 (TIA Portal) -- Creating S7 programs -- Loading and testing S7 programs
Why in STEP 7 (TIA Portal) V11 is the block comparison different although the networks are the same offline and online?
How do you do a program upload in STEP 7 (TIA Portal) V12 when the device has been configured withSTEP 7 V11?
Why in STEP 7 V11 are the online changes made to technology object parameters marked as retained not effective?
Why are blocks marked differently in the STEP 7 V11 Online View although they are identical?
How should you create a user-defined website in STEP 7 (TIA Portal) in order to control the CPU with an iPad?
How do you load a project into the CPU in STEP 7 (TIA Portal) V11?
In STEP 7 (TIA Portal) V11, how can you upload blocks from the CPU to the PG, for example, into a newly created project?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200 CPU is in operation (RUN)?
Why is communication between the Runtime simulation and the S7-1200 not possible if the PG/PC interface is not set correctly?
How do you transfer a program to an S7-1200 CPU without TIA Portal V11?
How can you have two online connections between STEP 7 V5.5 and an S7-300 and between STEP 7 V11 and an S7-1200 side by side?
In STEP 7 (TIA Portal), how do you download/upload a single data block into/out of the S7-1200 CPU without overwriting the monitored values?
STEP 7 -- Creating S7 programs -- Loading and testing S7 programs
How can you have two online connections between STEP 7 V5.5 and an S7-300 and between STEP 7 V11 and an S7-1200 side by side?
How can you switch between an S7 CPU and an S7 PLCSIM?
How can you display the messages in STEP 7 using the "CPU messages..." function?
Why should you switch the operating mode of the CPU from Test to Process after commissioning the STEP 7 program?
Tips and tricks for loading and testing S7 programs
How can I debug a STEP 7 program using the Breakpoint function?
How can you set up the online connection again between the PG and the CPU?
How can you change the startup and actual values only via the OP in such a way as to be immune to power failure and general reset?
How can you modify variables in STEP 7 version V5.2 and higher?
How can you monitor a block with the desired call environment in STEP 7?
Information about "Loading and testing S7 programs"
Why does the network status only appear partially during monitoring in the LAD and FBD editor?
What is the difference between offline and online processing in the LAD/STL/FBD editor?
How can you have two online connections between STEP 7 V5.5 and an S7-300 and between STEP 7 V11 and an S7-1200 side by side?
Part number:

Description
In STEP 7 V5.5 you can establish an online connection to an S7-300 or to an S7-400 and at the same time have an online connection between STEP 7 V11 and an S7-1200. In order to establish an online connection to the target systems you must assign the PG/PC interface an appropriate network access. The interfaces below are supported automatically:

  • MPI
  • PROFIBUS
  • Industrial Ethernet (ISO and TCP/IP)

Open the PG/PC interface in the SIMATIC Manager of STEP 7 V5.5 with the menu command "Options > Set PG/PC interface..." and in the "Interface Parameter Assignment Used:" window you select the access point for your online connection as in Fig. 01.


Fig. 01

In STEP 7 V11 all the active network accesses of your PG/PC are in the "Online" accesses area in the project navigation. Via the menu command "Go online" you can have all the available interfaces displayed in a list. In the "Go online" dialog you select the type of the PG/PC interface to establish the online connection.


Fig. 02

More information is available in the Online Help of STEP 711 under:

  • Connect PG/PC interface with a subnet
  • Assign an IP address to a PROFINET IO device
  • Go online with multiple devices
  • Define PG/PC interface, go online
  • Displaying accessible nodes

 Entry ID:50572734   Date:2011-06-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour