show the entry list
RFID / Moby -- Product information -- Technical data
Which communication modules are available for connecting the MOBY U identification system to the automation level?
What should you watch out for when using an ASM456 in a Y-link (IM153)?
How can you operate an RFID Reader on an ET 200S?
Why does the read/write device not recognize the Moby D transponder?
Why does the RFID standard block FB45 / FC45 report "error_bus 80A2" when using an RF170C?
Why is the data carrier RF320T sometimes only poorly recognized?
What should you do when error message E5 FE 06 is issued when operating MOBY U with RFID standard profile?
How can you operate readers (SLG) of RF300 and/or MOBY D via an ASM 400 in a SIMATIC S5?
Why does the RFID standard block FB45 / FC45 report "error_bus 80A2" when using an RF170C?
Part number:

Description:
When parameterizing the RF170C communication module, you must set the DP Alarm Mode of the ET200pro header module to DPV1.


Fig. 01

Unlike the other communication modules, the RF170C works only with DPV1.
If you use DPV0, you get error messages (error_bus 80A2) reported by the RFID standard block FB45 / FC45.

Detailed information is available in the operating instructions SIMATIC Sensors RFID systems RF170C communication module RF170C in Chapter 5 Parameter settings in Entry ID: 32622825.

 Entry ID:34515706   Date:2009-02-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour