show the entry list
SINAMICS G: Information on the standby current of the SINAMICS G120
Part number:

Task
In many applications, it is necessary to supply several frequency inverters from one infeed unit. The disadvantage of this type of power supply is the fact that the load as well as the no-load (standby) currents are summed - and both the infeed and power supply cables must be appropriately dimensioned.
An electric monorail (EMS) is a typical example of such a drive configuration. In the automobile industry, the EMS is an indispensable transport medium to ensure both flexible and rational material flow.

Solution
The behavior of the PM250 / PM250D Power Modules regarding the power and current drawn from the line supply is explained in the description. Using examples, it is shown how the current (apparent current) that the frequency inverter draws from the line supply can be calculated; for instance, when selecting the correct cross-section of power supply cables.

Downloads
Content of Downloads

Download

Documentation 34189181_Standby_currents_G120D_en.pdf ( 292 KB )
Excel-Tool G120D_standby_current_calculator_V2.zip ( 199 KB )

 

Additional Information
Title

Link

FAQ: SINAMICS G120D: Cascading the 24 Volt power supply of the CU240D Entry-ID: 26986267
FAQ: Where do I find information regarding the standby current of my SINAMICS G120D? Entry-ID: 31764702

Last Changes
Excel Tool replaced

 

Filter criteria:
Hardware platform: SINAMICS G, Distributed I/Os/ET200
Software: none
Entry contents: Background and system description
 Entry ID:34189181   Date:2012-09-05 
I regard this article....as helpfulas not helpful                                 
related links
MICROMASTER: Operating several mo ...
SINAMICS G: Speed control of a G1 ...
MICROMASTER/SINAMICS G: Displayin ...
SINAMICS G: Speed control of a G1 ...
MICROMASTER 4: operating MICROMAS ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
Contact
Support Request
Contacts worldwide
Technical Forum
QuickLinks
Compatibility tool 
Performance Data 
Micro Automation Sets
Help
Online Help
Guided Tour