show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication in the IWLAN in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Part number:

Description:
The IO link master module "4SI IO link" for the ET 200S distributed I/O system is included in the first version delivered in accordance with IOL standard V1.0. Up to four IO link devices (sensors and actuators) can be connected to the IO link master module.
The Port Configuration Tool (S7-PCT) is used to parameterize the IO link master module "4SI IO-Link" and the IO link devices. The S7-PCT is available to download in the following entry: 32469496.


Fig. 01: IO link system

If a device becomes defective and has to be replaced with a new one, the new device had to be reparameterized since new devices generally come with factory settings. If the function for reparameterizing replaced components is implemented in the system, the startup data which is saved in the host is sent to the lower-level components. This represents a system solution for replacing devices without having to connect the programming device (PG).

The reparameterization of replaced components is not implemented in the first version of the IO link system delivered; i.e. even though the IO link master parameters are saved on the IO link master module, replacing the IO link master module would necessitate reparameterization by means of S7-PCT. If an IO link device is replaced, there is also a need for reparameterization by means of S7-PCT because the IO link device parameters are only saved in the actual IO link device.

(Parameter) data is written to an IO link device or read from an IO link device with FB1, "IOL_CALL". The data is assigned a unique address on the IO link device with an index and subindex.

FB1 "IOL_CALL" and a description of FB1 "IOL_CALL" are available to download in the following entry: 32011237.

The block provides support with the following tasks:

  • (Re)parameterizing an IO link device during operation
  • Executing IO link port functions
  • Saving / Backing up IO link device parameters
  • Saving / Backing up IO link master parameters


Fig. 02: FB1 "IOL_CALL"

Using FB1 "IOL_CALL" to replace an IO link master and an IO link device without a PG
FB1 "IO_CALL" can be used to read any data objects from IO link devices, to save these objects so that they are powerfail-proof and to write to an IO link device again after replacing it by means of the FB1 "IO_CALL". The FB1 "IOL_CALL" and the retentive saving process must be controlled by the user program, e.g. by triggering the mechanism via a binary switch.

Since every IO link device contains other data objects, there can only be one user-specific solution in which the IO link device parameters have to be saved and backed up.

A special function of FB1 "IOL_CALL" can be used to save and back up the master parameters. If the input parameters "IOL_INDEX" and "IOL_SUBINDEX" are preconfigured with "0", the IO link master parameters are handled.

 Entry ID:33410269   Date:2009-01-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour