Requirements:
- Data media with original version of LOGO!Soft Comfort
(version lower than V5.0 SP3)
- Powerful Internet connection
Notes: LOGO!Soft Comfort V5.0 (SP3) onwards supports the Windows Vista operating system in all its versions (except 64 bit).
Installation instructions: All versions of LOGO! Soft Comfort lower than V5.0 SP3 need an upgrade for the installation.
The upgrades are available at the following link:
Upgrade for LOGO! Comfort V6
To ensure error-free installation, please make sure that the Setup.exe of the downloaded upgrade is executed on the Windows Vista user interface and not the setup of the original LOGO!Soft Comfort version.
|