show the entry list
RFID / Moby -- Product information -- Technical data
Which communication modules are available for connecting the MOBY U identification system to the automation level?
What should you watch out for when using an ASM456 in a Y-link (IM153)?
How can you operate an RFID Reader on an ET 200S?
Why does the read/write device not recognize the Moby D transponder?
Why does the RFID standard block FB45 / FC45 report "error_bus 80A2" when using an RF170C?
Why is the data carrier RF320T sometimes only poorly recognized?
What should you do when error message E5 FE 06 is issued when operating MOBY U with RFID standard profile?
How can you operate readers (SLG) of RF300 and/or MOBY D via an ASM 400 in a SIMATIC S5?
What should you do when error message E5 FE 06 is issued when operating MOBY U with RFID standard profile?
Part number:

Description:
The error message might be issued if MOBY U is used

  • with function block FB101/116/132,
  • with file handler mode set in the parameterization and
  • with the command READ, PHYSICAL READ or GET DIRECTORY.

Remedy:
Make sure that the maximum data record length of 240 bytes between ASM and SLG U 92 is not exceeded with the command. If you want to read longer data records from MDS, then you must execute the read command multiple times and read part of the data each time.

Keyword:
Filehandler

 Entry ID:27237305   Date:2008-05-15 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour