show the entry list
LOGO! Soft Comfort -- Setting up development environments -- Installing and upgrading software
Which SIMATIC software can you install in 64-bit operating systems?
How do you install LOGO!Soft Comfort (lower than V5.0 SP3) on Windows Vista?
Using LOGO! Soft Comfort in Mac OS 10.3 and Java 10.4.2
For which operating systems is LOGO! Soft Comfort released?
Why after a software upgrade/update in LOGO! Soft Comfort aren't the functions "Open..." and "Save as..." available any more in the File menu?
How with LOGO!Soft Comfort do you make an upgrade, update or extension?
What is the difference between update, upgrade and extensions?
Using LOGO! Soft Comfort in Mac OS 10.3 and Java 10.4.2
Part number:

Instructions:
When you start LOGO! Soft Comfort, the windows opens only briefly. It closes again after a few seconds.

Open LOGO! Soft Comfort with the command bar (the command bar is in the Terminal.atp under applications/utilities).
If the error message "Segmentation fault" is displayed, the behavior is due to Java crashing when opening LOGO! Soft Comfort.

Update your system using the "sudo update_prebinding -root' / -force" command entered in the terminal.

Keywords:
Logo, Mac OS, Logo Soft Comfort

 Entry ID:25447635   Date:2007-05-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour