show the entry list
WinCC flexible ES -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Message indicator continues to be displayed despite counter at zero
How do you start a sound file via a script in the WinCC flexible PC Runtime?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you determine the bit number in WinCC for the "Trigger address", the "Acknowledgement PLC" bit and the "Acknowledgement HMI" bit for creating bit messages?
Which configuration steps have to be taken in SIMOTION SCOUT and WinCC flexible to enable Alarm_S messages and technological alarms to be displayed in WinCC flexible Runtime?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
How do you display messages in WinCC flexible?
How can you evaluate the ACK button on a touch operator panel in WinCC flexible?
How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible?
How do you change and display SIMATIC WinCC flexible system events during configuration?
How can you change the ProTool default alarm window setting in WinCC flexible?
How can I acknowledge alarms in WinCC flexible via the PLC?
Why aren't messages output on the event recorder?
Why isn't the "Message display" shown in the foreground, but is covered by picture objects?
Why are no messages from the S7 diagnostics buffer display in WinCC flexible?
How can you get the diagnostics buffer to be displayed in WinCC flexible?
Which settings need to be made in order to display alarm events after a specified point in time?
How can you create messages with externally preset texts as mass data and process them with Excel in WinCC flexible?
Why are no messages from the S7 diagnostics buffer display in WinCC flexible?
Part number:

 

Description:
The S7 diagnostics puffer, as available in ProTool, is not support in WinCC flexible.
Diagnostics messages can be realized in WinCC flexible using the "SFM" (system error messages) function.

SFM is based on the Alarm_S alarm procedure. Here the panel receives significantly more detailed message texts than in the context of the diagnostics buffer.
Furthermore, the SFM messages are send actively (Alarm_S).
In comparison only very few diagnostic messages are actively sent by the CPU from the diagnostics buffer (e.g. CPU in Stop). If all the messages are to be displayed, then the operator must execute the "Read diagnostics buffer" function on the operator panel.

Entry ID 22319131 includes instructions on how to have system error messages of a SIMATIC S7-300 / 400 controller displayed in WinCC flexible.

If messages via SFM in the context of WinCC flexible is not sufficient and you need the S7 diagnostics buffer in addition, then Entry ID 22407622 includes instructions on how you can evaluate the S7 diagnostics buffer using the SFC 51 RDSYSST.
Using the SFC 51 you can output the S7 message numbers and the time stamp on an operator panel.


 Entry ID:22449810   Date:2006-01-09