Configuration Notes If you use a High Feature I/O module, then you do not necessarily have to use a High Feature interface module. Basically, you can use the ET 200S modules regardless of the version of the interface module used.
The scope of modules in the GSD files and in the STEP 7 hardware catalog is identical.
In the distributed I/O system there are the following versions of the interface module IM that can be combined at will with the latest electronic modules:
Entry ID 21406019 provides the structure limits for configuring ET 200S modules.
Note: Certain electronic modules cannot be used with the above-mentioned interface modules or only from a defined version onwards. A list of these electronics modules is given in the manual of the interface module concerned.
There are also I/O modules that can only be implemented after certain interface modules.
IM 151-1
| |
IM 151-1 BASIC |
IM 151-1 ST |
IM 151-1 FO |
IM 151-1 HF |
DP
master module |
- |
- |
- |
- |
| Reserve module |
x |
x1) |
x |
x |
| F modules 2) |
- |
- |
- |
x |
IM 151-3
| |
IM 151-3 PN |
IM 151-3 PN FO |
IM 151-3 PN HF |
DP
master module |
- |
- |
- |
| Reserve module |
x |
x |
x |
| F modules 2) |
- |
- |
x |
IM 151-7 / IM 151-8 CPU
| |
IM 151-7 CPU |
IM 151-7F CPU |
IM 151-8 CPU |
IM 151-8F CPU |
DP
master module |
x3) |
x4) |
x |
x |
| Reserve module |
x |
x |
x |
x |
| F modules 2) |
- |
x |
- |
x |
| 1) |
The reserve module can be used with IM 151-1 ST from MLFB 6ES7 151-1AA03-0AB0 onwards with option handling (see Entry ID: 21407118).
The reserve module cannot be used with the following IM 151-1 ST: 6ES7 151-1AA00-0AB0. |
| 2) |
More information on using F modules is available in the manual "ET 200S Distributed I/O System Fail-Safe Modules" in Entry ID: 12490437 |
| 3) |
From order number: 6ES7151-7AA10-0AB0 FW 2.1 |
| 4) |
From order number: 6ES7151-7FA01-0AB0 |
Note: Use the SIMATIC ET 200 Selection Tool to configure your ET 200S station. This configuration tool guides you simply and easily through the configuration of an ET 200S station and supports you in selecting the various components and matching accessories.
The SIMATIC Selection Tool is in the configuration tool overview of the Industry Mall under Automation Technology.
Industry Mall
|