Description: In the template a message
display has been configured for displaying the system and
operation messages. When a message is displayed, it is displayed in
the current picture without the message area being brought to the
foreground. The message display remains in the background and
therefore cannot be read properly, because the display of the
current picture and the message display overlap.
It would be desirable to have the message area in the foreground
of the current picture (regardless of which picture is active).
Remedy: Instead of configuring the message
display in the template you should configure an alarm
window with the option "Automatic display".
 ( 69 KB )
Fig. 01
|