show the entry list
WinCC -- Configuring and programming communication -- Communication to S7, use of fast AR_SEND
How can you use process-driven archiving in WinCC for a process tag with SFB37 (AR_SEND)?
How do you use SFB37 (AR_SEND) for process-driven archiving of process values in WinCC Tag Logging archives?
How can you achieve archiving cycles of less than 500ms in WinCC Tag Logging?
How can you tell that WinCC has received data from AR_SEND (SFB37)?
Where is the data archived that is transferred by AR_SEND (SFB37) to WinCC?
How can you ensure that the variables in AR_SEND (SFB37) have the same time stamp?
How can you ensure that the variables in AR_SEND (SFB37) have the same time stamp?
Part number:

Instructions:
In order to give the same time stamp to the data in function block AR_SEND you must parameterize the AR_SEND block accordingly (parameter unit (type)). Detailed information on parameterizing the AR_SEND block is available in the WinCC Information System (WinCC Online Help) under the keyword "AR_SEND: Data Block Structures - Structures and Parameters". Note the examples given there.


 Entry ID:21737406   Date:2005-07-04