Description:: For the messages select the option
Reported, so that messages can be reported on a
printer.
By default the following settings are displayed in WinCC
flexible ES after calling the discrete alarms via Project Tree
> Operator Panel > Alarm Management > Discrete
Alarms:
- Text
- Number
- Class
- Trigger Tag
- Trigger bit
Fig. 1: Default settings for discrete alarms
You have two options for selecting the Reported
option.
The following setting refers to discrete messages. The setting for
analog messages is identical.
Option 1
In the parameters of the discrete alarm concerned you can select
the Report option via
Properties > Process.
Fig. 2: Report setting in discrete alarms
Option 2
In the table view right-click the "gray
header". A new window opens in which you can select the
Reported option.
Fig. 3: Selection window
Once you have selected the "Reported" option, the new option is
displayed in the "header". Now you can assign the option
Reported Off/On to each message.
Fig. 4: Message reporting
|