Instructions: Proceed a follows to change the ProTool
default alarm window setting in WinCC flexible:
In WinCC flexible you set a "alarm window" in the
"Template" dialog. In the Properties of the "alarm window" you can
now define which alarm classes are to be displayed in this alarm
window. For example, you can also create multiple alarm windows and
assign an alarm class to each alarm window separately.
In order to have just the system alarms displayed, for example,
you proceed as follows.
In the project directory Pictures > Template
you insert an alarm window from the menu window Tools >
Advanced Object . You define the position and the devices of
the alarm window as you wish.
Below you see the basic settings. You can make other settings at
any time to suit our personal requirements.
- General:
Set the options boxes to:
- Display > Alarms > Pending alarms
- Alarm classes > System
Fig. 1: General
- Properties:
Set the options boxes to:
| Mode > Window > |
Automatic display |
|
Closable |
|
Resizable |
Fig. 2: Properties
The alarm window configured is now displayed automatically when
a system alarm occurs. The alarm window is closed again after the
time set in the project directory Alarms >
Settings > Alarm Settings.
Fig. 3: Alarm
settings ( 38 KB )
Displaying / closing layers In the example above
"Layer 1" has been assigned to the alarm window in the Properties
of the alarm window.
Fig. 4: Alarm window "Layer 1"
In the configuration interface the alarm window is displayed in
the background of newly created pictures. If you do not want this,
you can deselect Layer 1 in the Properties of the "Template"
picture by selecting Properties > Layers. Then the
alarm window concerned is closed and can then no longer be seen in
this configuration interface.
Fig. 5: Picture property "Template"
More detailed information is available in the Online Help under
the keyword "Working with layers".
|