show the entry list
PROFIBUS general -- Product information -- System description
Which PROFIBUS connectors can you use in Zone 1 or 2?
Start-up characteristics of DP configuration after power supply OFF/ON
Parameter DP Master System ID
Failure of a master in a multimaster system
PRB checker with the Windows language setting German (Switzerland) 
Sporadic bus error with SIMATIC OPs on distributed I/O under S5 masters
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
Using S7 Communication, MPI, FDL or FMS on a PROFIBUS master system with Power Rail Booster
Changing from EN50170 to DPV1
Which products can you use with an RS 485-IS segment?
What options exist for using the BT200 tester on the PROFIBUS?
Which terminology do you use for cyclic PROFIdrive communication?
Which manuals are available to download from Industry Online Support regarding the diagnostic repeater and the RS 485 repeater?
Communication between two IM151 CPUs
How can you print on just one page the network topology determined via the Diagnostics Repeater?
Transferring the registration key to another PC/PG
PROFIBUS network components (electrical/optical) -- Product information -- System description
Which PROFIBUS connectors can you use in Zone 1 or 2?
Which connector do you use to connect fiber-optic cables to the optical interface of network components and terminals?
Using the diagnostics repeater in PROFIBUS DP networks with data photoelectric barrier
LED of the RS485 Repeater
Which manuals are available to download from Industry Online Support regarding the diagnostic repeater and the RS 485 repeater?
ET 200iSP -- Product information -- Technical data
Which PROFIBUS connectors can you use in Zone 1 or 2?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
ET 200S (standard modules) -- Product information -- Technical data
What are the requirements for using the S7 routing function and which modules can you implement?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which PROFIBUS connectors can you use in Zone 1 or 2?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
ET 200S: Are there special requirements for ET200S when mounted on sheet metal plates?
ET200S: How many motor starters can be allocated to a power module?
ET 200S: How many motor starters can be allocated to a power module?
ET 200S: How many load feeders may be connected?
Calculating the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Baud rates for ET200S FO modules
Maximum power load for digital output modules
Minimum distance to the ET 200S front
How do you assign and identify thermocouples?
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?
ET 200M (standard modules) -- Product information -- Checking compatibility
Which PROFIBUS connectors can you use in Zone 1 or 2?
Y link: in spare parts case, only replacement of the defective IM157 is necessary
Which function modules (FM) can be used remotely in an ET 200M?
Which PROFIBUS connectors can you use in Zone 1 or 2?
Part number:

Description
The ET 200S and ET 200M distributed I/O systems may be used right into Zone 2. The ET 200iSP intrinsically safe distributed I/O system may be used right into Zone 1.

You can use the following PROFIBUS connectors for connecting the PROFIBUS network in Zone 2 (non-intrinsically safe PROFIBUS network).
 
30° outgoing cable unit
(max. 1.5Mbit/s)
35° outgoing cable unit
(max. 12Mbit/s)
90° outgoing cable unit
(max. 12Mbit/s)
6ES7 972-0BA30-0XA0 6ES7 972-0BA41-0XA0 6ES7 972-0BA52-0XA0
- 6ES7 972-0BB41-0XA01) 6ES7 972-0BB52-0XA01)
- 6ES7 972-0BA60-0XA0 6ES7 972-0BA12-0XA0
- 6ES7 972-0BB60-0XA01) 6ES7 972-0BB12-0XA01)
1) PROFIBUS connector has a PG socket

For connecting an ET200iS in Zone 1, you must configure the PROFIBUS network in this area as intrinsically safe. Therefore, the above-listed PROFIBUS connectors are not suitable.

Use the PB FC Standard Cable IS GP (order number: 6XV1831-2A) and the PROFIBUS connector 6ES7 972-0DA60-0XA0 to connect the ET 200iSP intrinsically safe remote I/O system to the PROFIBUS network.

The IK PI catalog ("PROFIBUS" chapter) contains the technical data, order data and the order numbers of other PROFIBUS bus cables and bus connectors.

IK PI Catalog

Warning
In order to set up an intrinsically safe PROFIBUS segment, it is imperative to use the RS 485-IS coupler.
The manual for the RS 485-IS coupler is available in Entry ID 29306413.

 Entry ID:17880484   Date:2010-03-25 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour