QUESTION: Why doesn't the ET 200S module DI 4xNAMUR
work when I configure it with STEP 7 V5.2?
ANSWER: Due to changes in function the ET 200S module
DI 4xNAMUR (6ES7 131-4RD00-0AB0) can only be configured completely
with STEP 7 V5.2 SP1.
All modules that have already been configured with STEP 7 V5.2
without Service Pack have to be deleted and reconfigured with STEP
7 V5.2 SP1 or higher.
Keywords:
System requirements, Hardware configuration, ET 200S DI
|