show the entry list
PROFIBUS PC CPs -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 95-U via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
PROFIBUS PC Software -- Configuring and programming communication -- Configuring connections
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via PROFIBUS in the SIMATIC NET Quick Start Collection?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 95-U via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Part number:

Instructions:
In this example, a CP5611 is used to establish the FDL connection with an S5 station on the PROFIBUS via the OPC server.

Note:
The procedure described here also applies for communication processors CP5613/14 A2, CP5621 and CP5511/CP5512.

General information:
The requirement is that one of the two following configuration tools is installed.

  • NCM PC: 
    NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project.
  • STEP 7:  
    STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.

Only one of these two configuration tools can be installed.

Please follow the instructions below for configuring the PC station.

Guide_FDLS5_OPC_e.pdf ( 2145 KB )

Keywords:  
FDL connection, Send, Receive, OPC server, SOFTNET S7, SOFTNET DP, CP5613 A2, CP5614 A2, CP5611 A2, CP5511, CP5512, CP5621  Guidelines,  LSAP, CP5431

 Entry ID:16733087   Date:2008-04-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour