show the entry list
Industrial Ethernet PC software -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
What should I watch out for when using an "S/R OPC Server" in the Fetch/Write service mode?
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do I create a Fetch/Write-connection (S5-compatible communication) to SIMATIC S7 for the SIMATIC NET-OPC Server via Ethernet with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
Industrial Ethernet PC CPs -- Configuring and programming communication -- Configuring connections
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC PC modules by way of the Industrial Ethernet using the ISO transport protocol?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
Industrial Ethernet S5 CPs -- Configuring and programming communication -- Configuring connections
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure an Ethernet connection for data communication between a SIMATIC 505 with CP1434 TCP and the SIMATIC 505 OPC server?
Commissioning and Configuring an ISO Transport Connection between the SIMATIC S5 and SIMATIC S7 via Industrial Ethernet
Configuring a transport connection (CP1430 TF/TCP) for simultaneous sending and receiving
Setting port number for the CP1430 TCP with TCP native
How do I set up an ISO connection between a SIMATIC 505 (CP1434) and a SIMATIC S7 (CP343-1) via INDUSTRIAL ETHERNET?
How do you configure a TCP connection on the S5 side (CP 1430 TCP)?
What are the basic things to watch out for when configuring a TCP connection?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
Part number:

Instructions:
In this example, a standard Ethernet network card is used for the S5-compatible communication with the S5 station using the FETCH and WRITE services via the OPC server.

Note:
The procedure described here also applies for communication processors CP1613, CP1512 and CP1612.

General Information:
You can choose between two different configuration tools:

  • NCM PC: 
    NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project.
  • STEP 7:  
    STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.

Only one of these tools can be installed.

Please follow the instructions below for configuring the PC station.

Guideline_FW_S5_e.pdf ( 2024 KB )

Keywords:  
Fetch/Write connection, Configuration, Guideline, OPC Server, SOFTNET S7, SOFTNET S7 Lean, S7-1613

 Entry ID:16697502   Date:2008-04-01 
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
Themen
Help
Online Help
Guided Tour