show the entry list
S7-400 CPU 41x -- Configuring and programming communication -- Configuring the PROFIBUS interface
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
What do you have to consider when connecting a S7-400 CPU to an external master as DP slave?
What differences are there when configuring S7 connections?
Transfer of analog values from and to the PROFIBUS DP slave
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
How can you tell whether your S7-300/400 master supports DPV1 functions?
Where are the settings of the MPI and PROFIBUS interfaces retained after updating the operating system for a CPU 41x?
PROFIBUS PC Software -- Configuring and programming communication -- Configuring connections
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 95-U via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
PROFIBUS PC CPs -- Configuring and programming communication -- Configuring connections
What differences are there when configuring S7 connections?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure a PC station as DP master for connecting to a DP slave for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software?
How do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 95-U via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S5 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
Information about "Configuring connections"
S7-300 CPU 31x -- Configuring and programming communication -- Configuring the PROFIBUS interface
How do you activate the "Prioritized OCM communication" function to improve the OP communication performance?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
What differences are there when configuring S7 connections?
Transfer of analog values from and to the PROFIBUS DP slave
What should you pay attention to when operating a DP slave temporarily on a PROFIBUS DP network?
How do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
What are the differences between the integrated DP interface of a CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
What are the options for exchanging data between CPUs via MPI/PROFIBUS DP?
Direct data exchange (internode communication) between two CPU modules
S7 routing via PROFIBUS with S7-300
Rules for accessing the CPU 315-2 DP on distributed I/O (integrated DP interface of CPU 315-2 DP)
Startup of the S7-300 CPUs when slave is not available
Routing with compact CPU and C7-635 as DP slave
How can you tell whether your S7-300/400 master supports DPV1 functions?
PROFIBUS S7-300/400 CPs -- Configuring and programming communication -- Configuring connections
How do you configure an FDL connection between the SIMATIC S5 (CP5431) and SIMATIC S7 via PROFIBUS?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure an FDL connection to the SIMATIC S7 via PROFIBUS for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
What differences are there when configuring S7 connections?
How do you configure a PC station as DP slave for connecting an S7 station (as DP master) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Part number:

Instructions:
In this example, a CP5611 is used for the communication via the OPC server as DP slave with an S7 station as DP master on the PROFIBUS.

Note:
The procedure described here also applies for communication processors CP5511, CP5512 and CP5621.

General information:
You can choose between two different configuration tools:

  • NCM PC:
    NCM PC is supplied with the SIMATIC NET CD and permits you to create PC projects and open STEP 7 projects. However, it is not possible to use this software to edit the S7 blocks in the STEP 7 project. 
  • STEP 7:
    STEP 7 is a separate software package and permits you to create S7-400, S7-300 and PC projects. It is possible to use this software to edit the S7 blocks.
The requirement is that STEP 7 is installed and that the DP master is already configured (for example, STEP 7 project with the configuration of an S7 station). If the DP master is also a PC station, then the configuration of the PC station as DP slave can also be made with NCM PC.

Please follow the instructions below for configuring the PC station.

Guide_DPSlave_e.pdf ( 1366 KB )

More information on using and configuring a PC station as DP slave or DP master is available in the applications listed below:
 
Title of application Entry ID
Distributed Automation with the PC - The SIMATIC NET OPC Server as PROFIBUS DP Slave 21040390
Controlling with the PC - The SIMATIC NET OPC Inproc Server as DP Master 21045282

Keywords:
DP-Slave, CP5611, CP5511, CP5512, CP5621, Hardware Configuration, SIMATIC NET PC software, Configuration, Guidelines, SOFTNET DP slave, Link DP slave, PC station.

 Entry ID:16650883   Date:2008-05-07