show the entry list
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
Touch Panel / Operator Panel -- Setting up systems -- Transferring projects
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
Which connector cables are available for connecting to SIMATIC Panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Transferring the configuration in the case of graphics-oriented devices
Transferring a configuration with Windows-based devices
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Screen disabling with OP27 and TP27
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
When editing the second OP language, variables are shifted in the other language.
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Part number:

QUESTION:
How can I assign headers to OP3 pictures so that the pictures are listed in the table of contents?

ANSWER:
In ProTool V5.2 / SP2 you can no longer assign headers to OP3 pictures. If you still want to assign a header to a picture so that it is displayed in the table of contents, then please proceed as follows:
Configure an empty picture for an OP7 and give this picture a header. Then copy it into an OP3 project. Now you can no longer change the header.

Note:
With ProTool V6, headers can be assigned.

Keywords:
Panels, Overview

 Entry ID:7878468   Date:2002-01-10