show the entry list
Touch Panel / Operator Panel -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Transferring the configuration in the case of graphics-oriented devices
Transferring a configuration with Windows-based devices
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Screen disabling with OP27 and TP27
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
When editing the second OP language, variables are shifted in the other language.
Transferring the configuration in the case of graphics-oriented devices
Part number:

QUESTION:
When replacing a graphics-oriented Touch/Operator Panel, how can I transfer the configuration to the new TP/OP?

ANSWER:
Using a storage card you can transfer the configuration without the ProTool configuration software. For this you slot the storage card into the relevant slot you’re your TP/OP and using the "Backup" function transfer all the data of the TP/OP (image of the TP/OP) onto the flash card.
With the power turned off, you slot this card into the new TP/OP. When you turn this TP/OP on, the configuration is transferred from the flash. Then using the "Restore" function you transfer the data from the storage card into the internal flash of the TP/OP.

 Entry ID:5869985   Date:2002-06-24 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour