show the entry list
WinCC (TIA Portal) -- Creating HMI configurations -- Loading and testing configurations
Why does communication not work between WinCC Professional Runtime and S7-1200?
Why do other WinCC stations not appear in the network environment on the Windows 7 and Windows Server 2008 PCs?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
How do you configure the Autostart for WinCC Runtime Advanced V11 in Windows 7 Embedded?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
With WinCC Engineering (TIA Portal), how can you transfer an HMI configuration without configuration software to an operator panel (Pack&Go)?
Comfort Panels -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
What transfer options are available in the various operator panels?
Multi Panel -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Touch Panel / Operator Panel -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
Transferring the configuration in the case of graphics-oriented devices
Transferring a configuration with Windows-based devices
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Screen disabling with OP27 and TP27
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
When editing the second OP language, variables are shifted in the other language.
Mobile Panels -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What transfer options are available in the various operator panels?
How do you back transfer the projects of an operator panel and what should you watch out for?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
Basic Panels -- Setting up systems -- Transferring projects
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?
Part number:

Description
The attached PDF document informs you about the settings needed to transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS.


Fig. 01

The document describes the following settings...

  • On the operator panel.
  • On the configuration PC.
  • In WinCC (TIA Portal).

Download
Documentation
 
WinCC V11 (TIA Portal) Project transfer

WinCC_V11_Panel_MPI_DP_Transfer_en.pdf ( 961 KB )

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Download, Transfer, Load, Control Panel, Channel, Remote Control, Commissioning, Project transfer, Bus address, Transmission rate, Device configuration, Bus parameters, Network settings, Network view, Connection, Nodes, PG/PC interface, Interface configuration

 Entry ID:58668002   Date:2012-03-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour