show the entry list
WinCC flexible ES -- Product information -- General information
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How do you make printouts on different printers in WinCC flexible PC Runtime?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
What are the functional differences between the different SIMATIC panels?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you send customer projects to Technical Support?
Why are PDF documents not displayed properly on the MP377?
Which GSD files are there for the Profibus DP operator panels?
Which GSDML files are there for the operator panels for Profinet IO?
Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels?
WinCC flexible RT -- Product information -- General information
Why does the "Lock program switching" function no longer work after upgrading from SIMATIC WinCC flexible Runtime 2008 SP2 to SP3?
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
What support does Siemens AG offer to make the use of WinCC flexible comply with FDA regulations?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
Which ports are used by WinCC flexible?
WinCC (TIA Portal) -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
Which SIMATIC software can you install in 64-bit operating systems?
Which devices and modules are supported by STEP 7 Professional V11 and WinCC Professional V11?
With what are SIMATIC WinCC V11 and WinCC V12 compatible?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
Part number:

Description
With the installation of Service Pack 3 for WinCC flexible 2008 on HP notebooks there are incompatibilities with the HP keyboard driver.

The following products are affected:

  • SIMATIC WinCC flexible 2008 SP3 Compact/Standard/Advanced
  • SIMATIC WinCC flexible 2008 SP3 Runtime

Products not affected:
New corrected DVDs have been supplied since May 2012 for WinCC Comfort/Advanced/Professional and WinCC Runtime Advanced. The corrected version is indicated by the overprint V11 SP2 SE incl. Update 2 on the DVD. This DVD eliminates the need for the procedure below.

Remedy
There are two alternatives for avoiding this incompatibility. Either you uninstall the HP keyboard driver or you uninstall the keyboard driver that is installed with WinCC flexible Runtime or the simulation.
Both alternatives must be executed at the latest before the concluding restart of the PC after installation of WinCC flexible 2008 SP3.

If the restart after installation has already been made and the system no longer starts or you have a blue screen, follow the instructions given under "Run_Windows_Repair".

The alternatives are described below each with their advantages and disadvantages.

  1. Uninstallation of the HP keyboard driver
  2. Uninstallation of the keyboard driver of WinCC flexible Runtime

1.
Uninstallation of the HP keyboard driver

With this alternative the task switching function is retained for WinCC flexible Runtime. Uninstallation of the driver might limit use of the HP special keys. To continue with this alternative you must uninstall the HP keyboard driver as follows before installing WinCC flexible 2008 SP3.
 
No. Procedure
1 Open the Windows Device Manager.


Fig. 01

2 Navigate to: Keyboards, "Standard ... Keyboard with HP QLB " right-click to open the Properties.


Fig. 02

3 Open the "Driver" tab and select Roll Back Driver for the HP keyboard driver.


Fig. 03

4 Acknowledge the dialog that opens with "Yes" and "OK".
The result is that the standard Microsoft keyboard driver is used.


Fig. 04

5 Quit the Device Manager and restart the PC.
Table 01

2. 
Uninstallation of the keyboard driver of WinCC flexible Runtime
This alternative retains the HP special key functions. Uninstallation of the driver disables the task switching function for WinCC flexible Runtime. To continue with this alternative you must uninstall the keyboard driver for WinCC flexible Runtime as follows before restarting the PC after installation of WinCC flexible 2008 SP3.
 
No. Procedure
1 Open the input prompt (CMD) with administrator rights.


Fig. 05


Fig. 06

2 Open the driver directory. The directory path for the driver directory depends on the installed operating system.

Driver directory on 32-bit operating systems:
"C:\Program Files\Common Files\Siemens\HmiRTmDriver32"

Driver directory on 64-bit operating systems:
"C:\Program Files\Common Files\Siemens\HmiRTmDriver64"


Fig. 07

3 Remove the driver with the following command:

For the WinCC flexible Runtime:
"FwKbdRTmRegister.exe -r fwkbdrtm -d fwkbdrtm.sys"


Fig. 08

4 Quit the Command Prompt and restart the PC.
Table 02

Run Windows Repair
If WinCC flexible 2008 SP3 is already installed and the ensuing restart already made, the system might no longer start or you get a blue screen.
Below is the procedure for this case.

Note
You need an additional USB keyboard for the steps below.
 
No. Procedure
1 Run a "Startup Repair" (displayed after boot problems) or start the HP notebook from the Windows DVD.
2 Select the "Launch Startup Repair" option after the "Startup Repair" or after the start from the Windows DVD.
3 Interrupt the "Startup Repair is checking your system for problems" message with "Cancel" (abort search).
4 Acknowledge the "Do you really want to abort?" question with "Yes".
5 Select the "View advanced options for system recovery and support" option.
6 Select the USB keyboard and log on.
7 Open the input prompt (CMD).
8 Switch to the driver directory ("C:\Windows\system32\drivers", for example).
9 Rename the HP driver: "ren hpqkbfiltr.sys hpqkbfiltr.sys_".
10 Quit the input prompt (CMD) and restart the PC.
11 Use the USB keyboard or USB mouse to continue with Alternative 1 or 2.
Table 03

 Entry ID:58217334   Date:2012-10-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour