|
DESCRIPTION:
The Hotfix 3 for the Drive ES PCS7 V7.0 SP1 software can be downloaded with immediate effect.
The existing Hotfix 3 includes supplements to the SINAMICS product range for the use of the module drivers and faceplates included in Drive ES PCS7 V7.0 SP1.
It goes without saying that the HF3 also comprises all functions of the previous hotfixes, that means, in particular the extensions of the HF2 regarding F-applications with F-systems are also included in HF3.
Details:
Without installing the HF3, you cannot interconnect the newest SINAMICS drives (such as G120C) from the SIMATIC PCS7 module driver wizard because the XML knowledge required for these SINAMICS drives has not yet been acquired. This XML knowledge is reinstalled by installing the HF3.
To ensure that all the new drives are also included in the PCS7/STEP7 hardware catalog, the new STARTER V4.2 or Drive ES Basic V5.5 must also be installed on the engineering PC additionally to this hotfix.
Installation requirements: This setup is a mere hotfix setup.
That means, the following installations are required as a minimum:
- Drive ES PCS7 V7.0 SP1 and
- SIMATIC PCS7 V7.0 SP3 (or later)
SINAMICS drives supported:
With the HF3, the module driver now supports the integration of the following SINAMICS drives, which can be performed conforming to the applicable standards via GSD files and TIA-conforming via the DriveES SlaveOM.
Note:
For SINAMICS G120 drives with CU 2xx-2 (firmware >4.x), the SINA_GS_Block must be used, for SINAMICS G120 drives with CU 2xx (firmware <4.x), the SINAG120.
Drives supported after installing the HF3:
- MICROMASTER 420
- MICROMASTER 440
- MICROMASTER 430
- MICROMASTER 411
- MASTERDRIVES CBP Vector Control
- MASTERDRIVES CBP Vector Control CUVC
- MASTERDRIVES CBP Motion Control
- MASTERDRIVES CBP Motion Control Plus
- MASTERDRIVES CBP Vector Control Plus
- MASTERDRIVES CBP2 Vector Control
- MASTERDRIVES Vector Control CUVC
- MASTERDRIVES CBP2 Motion Control
- MASTERDRIVES CBP2 Motion Control Plus
- MASTERDRIVES CBP2 Vector Control Plus
- CB15 MICROMASTER
- CB15 MICROMASTER Vector
- CB15 MIDIMASTER Vector
- CB155 COMBIMASTER
- DC - MASTER CBP DC MASTER
- DC - MASTER CBP2 DC MASTER
- DC - MASTER CBP SIMOTRAS HD
- DC - MASTER CBP2 SIMOTRAS HD
- SINAMICS DC MASTER
- SINAMICS S110 CU305
- SINAMICS S120 CU310
- SINAMICS S120 CU310-2
- SINAMICS S120 CU320
- SINAMICS S120 CU320-2DP
- SINAMICS SM120 CU320-2DP
- SINAMICS S150
- SINAMICS S150 CU320-2
- SINAMICS SL150 CU320-2
- SINAMICS G120 CU230P-2DP
- SINAMICS G120 CU240S
- SINAMICS G120 CU240S F
- SINAMICS G120 CU240D
- SINAMICS G120 CU240D F
- SINAMICS G120 CU240B-2DP
- SINAMICS G120 CU240E-2DP
- SINAMICS G120 CU240E-2DP F
- SINAMICS G120C G120C-DP
- SINAMICS G130
- SINAMICS G130 CU320-2
- SINAMICS G150
- SINAMICS G150 CU320-2
- SINAMICS GM150
- SINAMICS GM150 CU320-2
- SINAMICS GL150
- SINAMICS GL150 CU320-2
Drives with F-functionality (Safety Integrated) supported after installing the HF3:
- SINAMICS G120 CU240S DP F
- SINAMICS G120D CU240D DP F
- SINAMICS G120 CU240E-2DP F
- SINAMICS G120 CU240E-2DP
- SINAMICS G120C G120C-DP
- SINAMICS G130 CU320
- SINAMICS G130 CU320-2DP
- SINAMICS G150 CU320
- SINAMICS G150 CU320-2DP
- SINAMICS S110 CU305 DP
- SINAMICS S120 CU310 DP
- SINAMICS S120 CU310-2
- SINAMICS S120 CU320
- SINAMICS S120 CU320-2DP
- SINAMICS S150 CU320
- SINAMICS S150 CU320-2DP
How to install the HF3 for Drive ES PCS7 V7.0 SP1:
- Download the attached ZIP file "HF3_zu_DriveES_PCS7_V70_SP1.zip".
- Unpack the ZIP file into a target directory on your hard disk. Please ensure that no blanks are included in the path name of this target directory.
- After being unpacked, the shared directory must look as follows: \...\Disk1
- Double-click the \…\Disk1\SETUP.EXE to start the hotfix setup program.
More detailed information regarding Drive ES PCS7 V7.0 SP1 is included in the article ID: 39328969.
HF3_zu_DriveES_PCS7_V70_SP1.zip ( 2011 KB )
|