show the entry list

Comfort Panels -- Setting up systems -- Transferring projects 
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS? 
What transfer options are available in the various operator panels? 

How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS?Go to beginning
Part number:

Description
The attached PDF document informs you about the settings needed to transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS.


Fig. 01

The document describes the following settings...

  • On the operator panel.
  • On the configuration PC.
  • In WinCC (TIA Portal).

Download
Documentation
 
WinCC V11 (TIA Portal) Project transfer

WinCC_V11_Panel_MPI_DP_Transfer_en.pdf ( 961 KB )

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Download, Transfer, Load, Control Panel, Channel, Remote Control, Commissioning, Project transfer, Bus address, Transmission rate, Device configuration, Bus parameters, Network settings, Network view, Connection, Nodes, PG/PC interface, Interface configuration

What transfer options are available in the various operator panels?Go to beginning
Part number:

Transfer options
Attachment 1 lists the operator panels and their transfer options.

Attachment 1: Projecttransfer_V1_2_e.pdf ( 17 KB )    

USB host-to-host cables
More information on the topic of "USB host-to-host cables" is available in Entry ID: 19142034.

Application of adapters and cables
Attachment 2 indicates for each operator panel the plug-in cable required for the following applications:

  • Process coupling
  • Download (update operating system, project, ...)
  • Booting (filling in the case of a missing or damaged operating system)

Attachment 2: Panels_connecting_cables_V1_2_e.pdf ( 29 KB )  

Notes on USB PC adapter (6ES7972-0CB20-0XA0)and USB A2 PC adapter (6GK1 571-0BA00-0AA0)
The USB PC adapter/USB A2 PC adapter provides an MPI/DP interface through the PC's USB interface. More information about the USB PC adapter is available in the manual in Entry ID: 16983464 More information about the USB A2 PC adapter is available in the manual in Entry ID: 68849363
These cables are released only for the devices below for project transfer and OS updating.

  • OP 73
  • OP 77 A
  • TP 177 A
  • KTP600 Basic Color DP
  • KTP1000 Basic Color DP

Using USB RS232 adapters and USB Ethernet adapters
When using the RS232/PPI Multi-Master cable, zero modem cable or Ethernet connections, you can only use the "real" interfaces for project transfer.
"Real" interfaces are interfaces without implementation via USB. This means that you cannot use any "USB to serial" or "USB to Ethernet" adapters.

Additional Keywords
Project transfer, Project download, WinCC flexible, Transfer cable, ProTool, RS 232, PC/PPI cable, PC PPI cable, RS 485, Com Text, Cables, USB adapter

 Entry ID:51559631   Date:2013-05-03 
I regard this article....as helpfulas not helpful                                 






























related links
SIMATIC HMI WinCC flexible 2008 W ...
Which cable can you use for data ...
How can you transfer a WinCC flex ...
How can you transfer data via USB ...
Why do you get an error message w ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour