show the entry list
Delivery release for Drive ES Basic V5.5
Part number:
Summary Internet document

With immediate effect, the product Drive ES Basic V5.5 has been released for delivery.
This has been revised and enhanced due to the market launch of STEP7 V5.5, the support for the
operating system Windows 7 as well as an update of the integrated STARTER commissioning tool to Version V4.2.

Internet document Summary

Delivery release has been granted on April 5, 2011
 

Ordering information for Drive ES Basic V5.5

Order number

Designation

6SW1700-5JA00-5AA0

Drive ES Basic V5.5
Single license
6SW1700-5JA00-5AA1 Drive ES Basic V5.5
Copy license (60 users at the same time)
6SW1700-5JA00-5AA4 Upgrade Drive ES Basic V5.x --> V5.5
Upgrade license
6SW1700-0JA00-0AB2 Software Update Service (SUS) for
Drive ES Basic single license
6SW1700-0JA00-1AB2 Software Update Service (SUS) for
Drive ES Basic copy license

With immediate effect, the product Drive ES Basic V5.5 has been released for delivery.
This has been revised and enhanced due to the market launch of STEP7 V5.5, the support for the
operating system Windows 7 as well as an update of the integrated STARTER commissioning tool to Version V4.2.


The following individual innovations have been made in the V5.5 compared to the previous version V5.4 SP5:

  • Support for the operating system Windows 7 (32 Bit) in the versions Professional and Ultimate
  • Fully compatible with STEP7 V5.5
  • Starter Version V4.2, the commissioning tool for SINAMICS and MICROMASTER 4th Generation, has been integrated.
  • Communication to SINAMICS G120 drives with CU2xx-2 also supported via USB (native)
  • SimoCom A Version V 05.02.01, the tool for the POSMO A, has been integrated.
  • SimoCom U Version V 13.01.03, the tool for the SIMODRIVE 611U and POSMO CA/CD/SI, has been integrated.
  • DriveMonitor Version V5.4 SP3, the tool for MASTERDRIVES and SIMOREG, has been integrated. (unchanged)
     

Benefits provided by a Drive ES Basic installation compared to the installation of individual tools:

  • Benefits provided compared to all single tools (STARTER Stand alone, SIMOCOM U/A and DriveMonitor)
    • More convenient integration of the drives in the hardware configuration of SIMATIC S7 via
      object manager (SlaveOM and DeviceOM) instead of GSD files
    • Communication can also be set up beyond network boundaries by routing in the SIMATIC and SIMOTION stations.
      Without Drive ES, the individual tools can only communicate with drives that are connected to the same subnet
      (PROFIBUS, PROFINET) as the engineering PC/PG.
      Please read the routing notes!
    • The tools can be directly called up in a context-sensitive manner from the SIMATIC Manager.
      All the necessary network information is automatically transferred for routing.
       
  • Further advantages compared to DriveMonitor and SIMOCOM U/A
    • Data archiving in the S7 project
       
  • Another advantage compared to DriveMonitor
    • Direct communication via PROFIBUS
      Without Drive ES, the DriveMonitor can only communicate with the drives via USS protocol via a serial interface
      or via a PROFIBUS-OPC server

Routing notes:

Routing-capable modules support routing to the drives beyond network boundaries.

  • Routing in combination with SIMOTION:
    All SIMOTION modules support the functionality "Routing/S7-Routing", but not the functionality "Data record routing".
    Thus, new G120 devices cannot be reached via routing with a CU2xx-2 behind a SIMOTION.
  • Routing in combination with SIMATIC S7:
    The "S7 routing-capable" SIMATIC modules are listed in the article ID 584459 or directly in the hardware catalog of the STEP7 hardware configuration.
    For routing to the new G120 devices with CU2xx-2, you require SIMATIC modules which, additionally to S7-Routing, also support the functionality "Data record routing".


         Fig. 01: Information screen with routing data


Innovations regarding the integrated Starter V4.2:

The newly integrated Starter V4.2 ( V4.2.0.0 ) supports the following drive systems: 

  • MICROMASTER 4th Generation
  • SINAMICS DCM with Firmware V1.1 and V1.2
  • SIMATIC ET200S FC with Firmware V1.0.x and V3.0.x
  • SIMATIC ET200pro FC with Firmware V3.0.x
  • SINAMICS G110 with Firmware V1.0.x and V1.1.x
  • SINAMICS G110D with Firmware V3.3.x and V3.4.x
  • SINAMICS G120 with Firmware V2.0.x, V2.1.x, V3.0.x, V3.1.x, V3.2.x, V4.2, V4.3.0, V4.3.2 and (with SSP) V4.4
  • SINAMICS G120C with Firmware (with SSP) V4.4
  • SINAMICS G120D with Firmware V3.0.x, V3.1.x, V3.2.x
  • SINAMICS G130 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
  • SINAMICS G130 with Firmware V4.3.1, V4.3.2 and (with SSP) V4.4
  • SINAMICS G150 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
  • SINAMICS G150 with Firmware V4.3.1, V4.3.2 and (with SSP) V4.4
  • SINAMICS GM150 with Firmware V2.5.1, V2.6.1 and V2.6.2
  • SINAMICS GM150 with Firmware V4.3.1 and (with SSP) V4.4
  • SINAMICS GL150 with Firmware V2.5.1, V2.6.1 and V2.6.2
  • SINAMICS GL150 with Firmware V4.3.1 and (with SSP) V4.4
  • SINAMICS S110 with Firmware V4.1, V4.3.1, V4.3.2 and (mit SSP) V4.4
  • SINAMICS S120 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
  • SINAMICS S120 with Firmware V4.3.1, V4.3.2 and (with SSP) V4.4
  • SINAMICS S150 with Firmware V2.1.x, V2.2.x, V2.3.x, V2.4.x, V2.5.1, V2.6.1 and V2.6.2
  • SINAMICS S150 with Firmware V4.3.1, V4.3.2 and (with SSP) V4.4
  • SINAMICS SL150 with Firmware V4.3.1 and (with SSP) V4.4
  • SINAMICS SM120 with Firmware (with SSP) V4.4

Further information regarding the integrated Starter Version V4.2 is provided in the article ID 48586975

The integrated commissioning tools can also be downloaded individually from the Internet and can be used as a free upgrade for an existing Drive ES Basic V5.4 SPx installation.

How to obtain the new Drive ES Basic Version?

New order!
With this delivery release, all orders placed for the Version V5.5 will be delivered. The price remains unchanged compared to the previous versions.

For users who have already purchased a Drive ES Basic V5.x version!
They can order the upgrade version which is offered at a significantly lower price than the full version. 
Due to limited memory space, you cannot download the complete Drive ES Basic DVD V5.5.
This can only be ordered via the upgrade version which is offered at a significantly lower price than the full version. 

For users who have subscribed to the Software Update Service 6SW1700-0JA00-0AB2 resp. 6SW1700-0JA00-1AB2!
Users who have already subscribed to the Software Update Service will automatically receive the new version.
More detailed information regarding Software Update Service processing is provided in the article ID 13532008

Operating systems and STEP7 compatibility:
Drive ES Basic can be used with the following Microsoft operating systems:

  • MS Windows 2000 SP4
  • Microsoft Windows XP Professional SP2 *) and SP3
  • Microsoft Windows Server 2003 SP2
  • Microsoft Windows Server 2008  (without DCC)
  • Microsoft Windows VISTA Business SP1 (32-Bit) **)
  • Microsoft Windows VISTA Ultimate SP1 (32-Bit) **)
  • Microsoft Windows 7 Professional (32-Bit) incl. SP1
  • Microsoft Windows 7 Ultimate (32-Bit) incl. SP1
  • MS Internet Explorer V6.0 (or later)

*) limited test scope
**) strongly limited test scope, that means, you can install this only at your own risk after acknowledging the relevant warning.

Drive ES Basic can be used with the following STEP7 versions:

  • STEP7 V5.3 SP1 (or later)
  • STEP7 V5.4 SPx
  • STEP7 V5.5.

More detailed information regarding the compatibility is included in the article ID 18495518
 

Languages supported:

  • German
  • English
  • French
  • Italian
  • Spanish
     

Note:
In Version V5.5 (or later), Drive ES Basic is only provided as a mere option package for SIMATIC STEP7, that means the Drive ES Basic V5.5 (or later) can only be installed additionally to an already installed STEP7 full version.
The procedure remains the same for SIMATIC-S7 users.

The Version V5.5 can, however, no longer be used with a STEP7 independent stand-alone installation.
The stand-alone installation is no longer supported as from the Drive ES Basic Version V5.5.

 

Product cancellation for the product Drive ES Basic V5.3

Upon release of the new Version V5.5, all previous versions are discontinued and phased out.
This means that the ordered units affected are no longer listed in the catalog, but will still be delivered as a spare part for approx. one year:
 
Order number Designation
6SW1700-5JA00-3AA0 Drive ES Basic V5.3 SPx
Single license
6SW1700-5JA00-3AA1 Drive ES Basic V5.3 SPx
Copy license (60 users at the same time)
6SW1700-5JA00-3AA4 Upgrade Drive ES Basic V5.x --> V5.3 SPx
Upgrade license

 

For more detailed information, please contact your local Siemens office.

 Entry ID:49578285   Date:2011-04-14 
I regard this article....as helpfulas not helpful                                 
related links
SINAMICS MICROMASTER STARTER
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour