show the entry list
STEP 7 (TIA Portal) -- Creating S7 programs -- Executing operations
How do you filter only the places before and after the decimal point from a real value in STEP 7 (TIA Portal) V11?
How do you calculate the linear values for the y-coordinate of point P in STEP 7 (TIA Portal) V11?
How can you add together physical flow measurements (mass flow rate, for example) to a total value in STEP 7 (TIA Portal) V11?
How do you implement numerical differentiation in STEP 7 (TIA Portal) V11?
How do you convert data types in the TIA Portal for the S7-1200/1500?
How can you convert a hexadecimal number into ASCII characters with STEP 7 (TIA Portal) V11?
How can you determine the bit position of an active bit in a marker word with STEP 7 V11 and monitor a 32-bit field?
How can you delay the output signal in relation to the input signal in STEP 7 (TIA Portal) V11?
In STEP 7 (TIA Portal) V11, how can you scale integer values in real numbers and real values in integer numbers for analog measurements?
How do you copy memory areas in STEP 7 (TIA Portal) V11?
How in STEP 7 V11 can you access the unstructured data types bit-by-bit, byte-by-byte or word-by-word and symbolically?
How do you program the overlapping of tags with the keyword "AT" in the TIA Portal V11?
How do you program a pulse encoder in STEP 7 (TIA Portal)?
How do you program a shift register with the LAD/FBD statements in STEP 7 V5.5 and in V11?
What properties do you have to watch out for in STEP 7 V11 when you are inserting characters into a string with the "INSERT" statement?
How can you add together physical flow measurements (mass flow rate, for example) to a total value in STEP 7 (TIA Portal) V11?
Part number:

Description
The STEP 7 (TIA Portal) V11 program "STEP7_V11_Totalizer" includes the "Totalizer" function block which you can use to add up values measured within a time unit to a total value. For example, for using units of measurement for linear velocity or for volumetric magnitudes. You can use distances or volumes as physical magnitudes and milliseconds, seconds, minutes, hours or days as units of time measurement.


Fig. 01

Table 01 below includes a list of the input and output variables of the "Totalizer" function.
 
Parameter Variable Data type Description
Input Value Real Measured value in a time interval
Input Interval Time Time interval of the measurement
Input Cycle Time Sampling time
Input Reset Bool Reset of the "Total" output
Output Total Real Accumulated total output value
Table 01

In a cycle

  1. The values of the input variables "Interval" and "Cycle" of the data type Time are converted into the data type Real.
  2. The converted values are then transferred to the temporary variables "Interval_real" and "Cycle_real".
  3. The input value of the variable "VALUE" is multiplied by the value of the temporary variable "Cycle_real" and then divided by the value of the temporary variable "Interval_real".
  4. The result is then stored in the buffer of the static variable "Accum".

Thus after each cycle the interim result in the "Accum" buffer is incremented by this value, which is also transferred to the output variable "Total". If the "Reset" variable has the value "True", the output value of the "Total" variable is reset to zero.

Example:
In the example as in Fig. 01 the "Value" variable has the value 60.0 and the time value of the "Interval" variable is one minute.

  • The output variable "Total" is then added up to the values 1 to 60 within the interval, that is to say within one minute.
  • The cycle time of 100ms reflects the scan time in which the FB "Totalizer" is processed.
  • When the FB is called in the "Cyclic interrupt", the program is processed in a time interval of 100ms and is independent of OB1 (main).

The associated physical units of the measured value "Value" can be, for example, meters per second, cubic meters per minute or kilograms per hour. For the input variable "Interval" you must enter the interval time for the physical unit, for example,

  • Meters per second: T#1s
  • Cubic meters per minute: T#1M
  • Kilograms per hour: T#1h


Fig. 02

The attached download "STEP7_V11_Totalizer.zip" contains a STEP 7 project with the blocks described above (FB "Totalizer" with instance DB and call in the "Cyclic interrupt" OB). The program contains German and English comments.

Copy the "STEP7_V11_Totalizer.zip" file into a separate directory and then start the file with a double-click. The STEP 7 project is now unpacked automatically with all the associated subdirectories. You can then use STEP 7 V11 to open and process the extracted project.

STEP7_V11_Totalizer.zip ( 9206 KB )

Creation environment
The screens and download in this FAQ response were created with STEP 7 (TIA Portal) V11 SP2.

 Entry ID:48799854   Date:2012-05-22 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour