show the entry list
How Do I Connect Sitrans FUS060 Pulse Output With Sitrans FUE950 (7ME347 only) Pulse Input And Set Up The Pulse Output?
Part number:

QUESTION:  

How Do I Connect Sitrans FUS060 Pulse Output With Sitrans FUE950 (7ME347 only) Pulse Input And Set Up The Pulse Output?

ANSWER:  

NOTE:
Only valid for FUE950 versions from 01-2010 with order code 7ME347.

Connect FUS060 and FUE950 as follows:
-           FUS060 terminal 5 (+) to FUE950 terminal 10 (pulse)         
-           FUS060 terminal 6 (-) to FUE950 terminal 11 (-)

Set up the Pulse output in FUS060 Transmitter Menu 4 (device outputs)
The pulse output  settings must be identical with the FUE950 pulse input settings. Also ensure that the pulse settings correspond to the information on the FUE950 type plate.

For further information about connection and setup of pulse output/input, refer to the attached PDF

Download printerfreindly version (pdf)
How Do I Connect Sitrans FUS060 Pulse Output With Sitrans FUE950 Pulse Input And Set Up The Pulse Output? ( 82 KB )


Download attached pdf file

Further information about connection and setup of pulse output/input ( 104 KB )

 Entry ID:44373327   Date:2010-06-28 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour