|
Question: How to complete the project?
Answer:
The missed MCC calls can be copied from the standard project for STS. This means that the SIMOTION Scout must be opened two times and the following programs must be copied from the STS standard project to the OHBC standard project: Gantp_1, Gantp_2, Trollp_1, Trollp_2 and Mon_Ref
A complete standard project for OHBC can be downloaded in following.
SIMOCRANE_BasicTechnologyApplication_OHBC.zip ( 2926 KB )
|