show the entry list
SIMOCRANE Basic Technology
SIMOCRANE: Load change of power semiconductors
SIMOCRANE Basic Technology – Getting Started and Tips for commissioning
SIMOCRANE Basic Technology: Slack rope controller and Current equalization controller
SIMOCRANE Basic Technology: Changes in SIMOCRANE Basic Technology V2.0 SP2
SIMOCRANE Basic Technology: Axis without encoder
SIMOCRANE Basic Technology : Switchover between Trolley and Boom
SIMOCRANE: SIMOTION RT-License
SIMOCRANE: Long delay time between switch off and on with the pulse enable
SIMOCRANE: IPO-overflow
SIMOCRANE: Upgrade Scout and Simocrane application project
SIMOCRANE: Assignment of DP address at DRIVE-CLiQ slots on Simotion D435
SIMOCRANE: DRIVE-CLiQ - clock synchronization
SIMOCRANE: Link to Cranes Application Notes and SIMOCRANE Standard applications and Tools
SIMOCRANE: Application with SINAMICS V2.6 SP2 and SIMOCRANE Basic Technology
SIMOCRANE: Offset-Mode in synchronous operation
SIMOCRANE: Switch over one motor between two drives (Motor Modules)
SIMOCRANE: Set the actual position automatically after Power-On
SIMOCRANE: Output-choke in switch-over one drive between two motors
SIMOCRANE: Problem in Standard project for Overhead Bridge Crane (OHBC)
SIMOCRANE Basic Technology: Failure detection on Active Line module in parallel operation
SIMOCRANE: Output-choke in switch-over one drive between two motors
Part number:

Question:
How to configure the output filter for a motor-module with switchover function?

Answer:
If we have different configurations to the motor module due to switch-over function, then the parameter p0230 ‘Drive filter type, motor side’ is set to ‘0’ = no filter. We must used the parameter p0353 [0...n] ‘Motor series inductance’ to adjust the used configuration with or without output choke. This parameter is dependent of the drive data set, refers to the schematic figure.

 Entry ID:43998451   Date:2010-07-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour