show the entry list
Evaluation of WinCC diagnostic files with proposals for solutions through help texts and online contributions of the Service & Support pages with the SIMATIC Analyser tool
Part number:

Task
In production plants with modern automation technology, high availability of plants and production processes are elementary. In contrast, faults and in the worst case, downtimes are to be avoided or at least limited to an acceptable level.

To achieve this, the diagnostic files of the SIMATIC products help to detect possible errors at an early stage. This can be especially the case when these diagnostic files are provided in a clear way and they are supplemented by the respective Online help.

Solution
The "SIMATIC Analyser" supports you in the analysis and early avoidance of possible errors. With this tool it is possible to read-in and analyze several diagnostic files, and to display them in a uniform format.
Apart from typical entries in the diagnostic files, entries from the Online Support are also offered next to help texts. This enables you to identify potential problems at an early stage and to initiate counter measures.

Function principle
The "SIMATIC Analyser" uses a two-step concept:

  • Collecting diagnostic files with the SIMATIC Diagnostics Tool. (Entry ID 44029135)
  • Analyzing the diagnostic files by comparing the entries with the database of the "SIMATIC Analyser".

Prerequisites
For the operation of the "SIMATIC Analyser" additional software is required. Information on this issue can be found in the help of chapter "Prerequisites for the use of the SIMATIC Analyser".

Downloads
Contents of the downloads

Download

Documentation
SIMATIC Analyser help.zip
SIMATIC_Analyser_V1_2_Help_76.zip ( 507 KB )
Code
SIMATIC Analyser V1.2.zip (help document included)
SIMATIC_Analyser_V1_2.zip ( 1916 KB )

 Additional information
Title

Link

How can I summarize the diagnostic and system information of my computers on a central computer? Entry ID: 44029135

Your feedback regarding the further development of the SIMATIC Analyser
Have you detected new diagnostic entries during your research and added them to your own database?
Please help us and send us your database to the following e-mail address: "online-support.industry@siemens.com". Use "SIMATIC Analyser Database" as subject.
Thank you very much!

History
Version

Changes

02/2011 First issue (SIMATIC Analyser V1.0)
11/2011 Function expansion with SIMATIC Analyser V1.1
03/2012 Function expansion with SIMATIC Analyser V1.2

Supplementary Search terms
Diagnostics Files,  DiagnosticsFiles, Log Files, LogFiles, SDT, analyzing, scanning, checking, diagnostics data, troubleshooting, error, error codes, dump file, crash, memory hog, script error, error message, diagnostics entry, PDLRTSEH.LOG, WinCC_Op_.log, SIMATIC_S7_Protocol_Suite_.LOG, WinCC_SStart_.log, WinCC_Sys_.log, event logs, 44029135, error search

Filter criteria:
Hardware platform: none
Software: WinCC up to V7.x
Entry contents: Function blocks/tools
 Entry ID:38645769   Date:2012-03-28 
I regard this article....as helpfulas not helpful                                 
related links
Are there lists for the compatibi ...
Wizard for Creating the Parameter ...
CEMAT V6.0 ServicePack 2 Now Avai ...
CEMAT V6.0 ServicePack 3 Now Avai ...
SIMATIC HMI Communication for Win ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
Contact
Support Request
Contacts worldwide
Technical Forum
Login VIP e-mail box
QuickLinks
Compatibility tool 
Performance Data 
Micro Automation Sets
Help
Online Help
Guided Tour