show the entry list
WinCC flexible ES -- Working with projects -- Importing / exporting data
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How can you import/export configuration data (discrete and analog alarm messages, tags and connections) from/to a CSV file in WinCC flexible 2008?
How can you create flexible text lists in WinCC flexible for export by drag-and-drop?
How can you import tags from data blocks and from the symbol table into WinCC flexible version 2005 and higher?
WinCC flexible ES -- Creating HMI configurations -- Loading and testing configurations
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
What can be the causes of the project download via TeleService not working?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
How can you transfer a WinCC flexible project serially to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you simulate with WinCC flexible the function keys of the various Windows-based operator panels via the PC keyboard?
Which cable can you use for data transfer between a Micro Panel and a configuration PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
Part number:

Description
With WinCC flexible as from 2008 SP1 you can use the "Pack&Go" function to create a file with which you can transfer an HMI configuration to an operator panel without any configuration software.

The "Pack&Go" file contains:

  • The compiled project
  • A program for transferring the project to the operator panel

Typical application
A configuration office creates a project for a new operator panel. The configuration engineer from the configuration office does not have direct access to the plant. Therefore, the configuration engineer sends the "Pack&Go" file per e-mail to his/her contact on site.
The contact unpacks the "Pack&Go" file on a PC that is linked to the operator panel over a network. Then he/she transfers the project from the PC to the operator panel.


Fig. 01

Notes

  • The version of the configured operator panel must match the operating system image of the operator panel. If necessary use ProSave to do an OS update.
    More information about doing an OS update is available in
    Entry ID: 19701610.
  • If the project is to be transferred via USB, you need a USB master-master cable. More information about USB transfers is available in Entry ID: 19109408
  • If the project is to be transferred over PROFIBUS, the hardware interface and driver must be installed on the transfer PC. The driver for an MPI/PROFIBUS card is also installed by ProSave, among others. You can download ProSave in Entry ID: 10347815
  • If you have Vista installed on your transfer PC and you want to transfer the project to an operator panel running the Windows CE operating system, you need administrator rights.
    It is not possible to use "Pack&Go" for transfer via Routing.

Operator panels supported
 
Micro Panels   OP 73micro
  TP 177 
Mobile Panel Mobile Panel 177
  Mobile Panel 277
  Mobile Panel 277 IWLAN
  Mobile Panel 277 IWLAN V2
Basic Panel

KP300 Basic

 

KTP400 Basic

 

KTP600 Basic

 

 KTP1000 Basic

 

TP1500 Basic

Panel OP 73, OP 77A, OP 77B
  OP / TP 177
  OP / TP 277
Multi Panel MP 177
  MP 277
  MP 377

Additional Keywords
Panels, Project download, Pack & Go

 Entry ID:36305011   Date:2013-05-21