show the entry list
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How can you save WinCC flexible projects / libraries as projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
What transfer options are available in the various operator panels?
How can you save WinCC flexible projects / libraries as projects / libraries in the format of an earlier version of WinCC flexible?
Part number:

Introduction:
In WinCC flexible (from WinCC flexible 2005), it is possible to save the current project also in the format of earlier versions of WinCC flexible. Libraries can also be saved in the format of earlier versions.

Requirements:

  • You have opened a project in the current version of WinCC flexible.
  • You have installed the "Support "Save as version"" component (only necessary as from WinCC flexible 2008).


Fig. 01

Procedure:
In the "Project" menu you select the "Save as version" command. In the dialog that opens you select the storage location, project name and version into which you wish to convert the project. Then you confirm with the "Save" button.


Fig. 02

You can also save libraries in the format of earlier versions. For this you right-click the library and select the appropriate dialog via the path "Library...> Save as version...". In this dialog you select the storage location, library name and version into which you wish to convert the project. Then you confirm with the "Save" button.


Fig. 03

Notes:

  • In Windows Vista it is not possible to save projects / libraries in the format of an earlier version of WinCC flexible, because the MSDE (Microsoft SQL Server Desktop Engine) is not available for Windows Vista.
  • If you save a WinCC flexible project / library from the current version in the format of an earlier version of WinCC flexible, there might be differences in the appearance and function of some objects.
  • Note that you can only save the configuration by one version lower (V-1) than the project file.
    Sometimes a Service Pack is considered to be a separate version. For example, in WinCC flexible 2007 it is only possible save as version WinCC flexible 2005 SP1.

More information on handling the different versions of WinCC flexible is available in Entry ID: 28531852.

 Entry ID:33934262   Date:2009-01-15 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour