|
1. SIMATIC NET Software Products Edition 2008 for PCs
1.1 PROFIBUS Software Products Edition 2008
|
Product |
Version/Edition |
Order No. |
|
S7-5613 |
2008 |
6GK1713-5CB71-3AA0 |
|
DP-5613 |
2008 |
6GK1713-5DB71-3AA0 |
|
FMS-5613 |
2008 |
6GK1713-5FB71-3AA0 |
|
SOFTNET-S7 * |
2008 |
6GK1704-5CW71-3AA0 |
|
SOFTNET-DP |
2008 |
6GK1704-5DW71-3AA0 |
|
SOFTNET-DP Slave |
2008 |
6GK1704-5SW71-3AA0 |
|
CP5613/CP5614 driver software / DP Base interface |
2008 |
-no order no.-
supplied together with CPs
(order no. of the CPs: 6GK1561-3FA00; 6GK1561-3AA01; 6GK1561-4AA01) |
* Please read entries in the readme of the CD ROM.
1.2 INDUSTRIAL ETHERNET Software Products Edition 2008
|
Product |
Version/Edition |
Order No. |
|
S7-1613 * |
2008 |
6GK1716-1CB71-3AA0 |
|
S7-REDCONNECT * |
2008 |
6GK1716-0HB71-3AA0 |
|
S7-REDCONNECT Power Pack* |
2008 |
6GK1716-0HB71-3AC0 |
|
TF-1613 |
2008 |
6GK1716-1TB71-3AA0 |
|
SOFTNET-S7* |
2008 |
6GK1704-1CW71-3AA0 |
|
SOFTNET-S7 Lean * |
2008 |
6GK1704-1LW71-3AA0 |
|
SOFTNET-PG |
2008 |
6GK1704-1PW71-3AA0 |
* Please read entries in the readme of the CD ROM.
Special with SOFTNET-S7 Lean for IE :
The quantity framework is limited to 8 connections. The scope of supply of SOFTNET-S7 Lean includes the SIMATIC NET OPC Server.
1.3 PROFINET Software Products Edition 2008
|
Product |
Version/Edition |
Order No. |
|
PROFINET CBA OPC-Server |
2008 |
6GK1706-0HB71-3AA0 |
|
SOFTNET PROFINET IO |
2008 |
6GK1704-1HW71-3AA0 |
Please note when you use PROFINET products
PROFINET CBA requires the iMAP configuration tool. iMAP is a separate product and must be ordered separately.
1.4 SNMP Software Products Edition 2008
|
Product |
Version/Edition |
Order No. |
Remark |
|
SNMP OPC-Server Basic |
2008 |
6GK1706-1NW71-3AA0 |
Administration of up to 20 IP addresses; |
|
SNMP OPC-Server Extended |
2008 |
6GK1706-1NX71-3AA0 |
Administration of up to 200 IP addresses; |
|
SNMP OPC-Server Power Pack |
2008 |
6GK1706-1NW71-3AC0 |
Expansion from Basic to Extended; |
The SNMP OPC-Server software enables access to SNMP-compatible devices in OPC-Client systems. This permits you to diagnose individual devices, going up to the complete plant, as well active control of device features. The extent and type of the diagnostic information and the control parameters depend on the individual scope of functions of the SNMP device.
1.5 DX OPC Server
Please note that the supply of the DX OPC Server has been discontinued effective October 01, 2008 (see entry ID 31507617). Edition 2008 (and subsequent) of this software will thus not be available.
1.6 SIMATIC NET S7-OPC-Server, Data Access on S7-OPC symbolic items of type ATI
The “IOPCItemIO“ OPC Data Access V3.0 interface for groupless reading and writing of S7-OPC symbolic items of type ATI has not been released for use. The “IOPCBrowse“ OPC Data Access V3.0 interface for browsing of the name area and for reading out item IDs and properties of S7-OPC symbolic items of type ATI is not released for simultaneous operation with several OPC Clients.
This information is also included with the affected products on a separate note.
We will inform you about a possible later release of the above functions via a separate bulletin.
1.7 Further details on the PC Software CD Edition 2008
Detailled information on the new version of the SIMATIC NET PC Software can be found in the files Liesmich ( 611 KB ) / Readme ( 530 KB ) which are also included on the SIMATIC NET CD Edition 2008.
The SIMATIC NET PC Software der Edition 2008 is now also released for use in SIMOTION applications. However, due to lack of time, this information is not included in the Liesmich/Readme files on the CD.
2. Upgrades and Software Update Service (SUS)
A specific Software Update Service for each SIMATIC NET PC product is available together with Edition 2008; it includes the supply of uprade packages.
This service is independent of the current version, so that the order no.’s of the individual SUS packages are the same as for 2007:
|
SOFTWARE Update Service for |
Order No. |
|
SIMATIC NET IE SOFTNET-S7 |
6GK1704-1CW00-3AL0 |
|
SIMATIC NET IE SOFTNET PN IO |
6GK1704-1HW00-3AL0 |
|
SIMATIC NET IE SOFTNET-S7 LEAN |
6GK1704-1LW00-3AL0 |
|
SIMATIC NET IE SOFTNET-PG |
6GK1704-1PW00-3AL0 |
|
SIMATIC NET PB SOFTNET-S7 |
6GK1704-5CW00-3AL0 |
|
SIMATIC NET PB SOFTNET-DP |
6GK1704-5DW00-3AL0 |
|
SIMATIC NET PB SOFTNET-DP-SLAVE |
6GK1704-5SW00-3AL0 |
|
SIMATIC NET IE PN CBA OPC-SERVER |
6GK1706-0HB00-3AL0 |
|
SIMATIC NET IE SNMP OPC-SERVER BASIC |
6GK1706-1NW00-3AL0 |
|
SIMATIC NET IE SNMP OPC-SERVER EXTENED |
6GK1706-1NX00-3AL0 |
|
SIMATIC NET PB S7-5613 |
6GK1713-5CB00-3AL0 |
|
SIMATIC NET PB DP-5613 |
6GK1713-5DB00-3AL0 |
|
SIMATIC NET PB FMS-5613 |
6GK1713-5FB00-3AL0 |
|
SIMATIC NET, S7-REDCONNECT |
6GK1716-0HB00-3AL0 |
|
SIMATIC NET IE S7-1613 |
6GK1716-1CB00-3AL0 |
|
SIMATIC NET IE TF-1613 |
6GK1716-1TB00-3AL0 |
Furthermore, the following separate upgrade packages are available for each SIMATIC NET PC product of Edition 2008:
|
SIMATIC NET IE SOFTNET-S7
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1704-1CW00-3AE1 |
|
SIMATIC NET IE SOFTNET-S7
UPGRADE for EDITION 2006 and higher |
6GK1704-1CW00-3AE0 |
|
SIMATIC NET IE SOFTN.PN IO
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1704-1HW00-3AE1 |
|
SIMATIC NET IE SOFTN.PN IO
UPGRADE for EDITION 2006 and higher |
6GK1704-1HW00-3AE0 |
|
SIMATIC NET IE SOFTNET-S7 LEAN
UPGRADE for V6.1, V6.2 and EDITION 2005 |
6GK1704-1LW00-3AE1 |
|
SIMATIC NET IE SOFTNET-S7 LEAN
UPGRADE for EDITION 2006 and higher |
6GK1704-1LW00-3AE0 |
|
SIMATIC NET IE SOFTNET-PG
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1704-1PW00-3AE1 |
|
SIMATIC NET IE SOFTNET-PG
UPGRADE for EDITION 2006 and higher |
6GK1704-1PW00-3AE0 |
|
SIMATIC NET PB SOFTNET-S7
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1704-5CW00-3AE1 |
|
SIMATIC NET PB SOFTNET-S7
UPGRADE for EDITION 2006 and higher |
6GK1704-5CW00-3AE0 |
|
SIMATIC NET PB SOFTNET-DP
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1704-5DW00-3AE1 |
|
SIMATIC NET PB SOFTNET-DP
UPGRADE for EDITION 2006 and higher |
6GK1704-5DW00-3AE0 |
|
SIMATIC NET PB SOFTNET-DP-SLAVE
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1704-5SW00-3AE1 |
|
SIMATIC NET PB SOFTNET-DP-SLAVE
UPGRADE for EDITION 2006 and higher |
6GK1704-5SW00-3AE0 |
|
SIMATIC NET IE PN CBA OPC SERVER
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1706-0HB00-3AE1 |
|
SIMATIC NET IE PN CBA OPC SERVER
UPGRADE for EDITION 2006 and higher |
6GK1706-0HB00-3AE0 |
|
SIMATIC NET IE SNMP OPC SERVER BASIC
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1706-1NW00-3AE1 |
|
SIMATIC NET IE SNMP OPC SERVER BASIC
UPGRADE for EDITION 2006 and higher |
6GK1706-1NW00-3AE0 |
|
SIMATIC NET IE SNMP OPC SERVER EXTENED
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1706-1NX00-3AE1 |
|
SIMATIC NET IE SNMP OPC-SERVER EXTENED
UPGRADE for EDITION 2006 and higher |
6GK1706-1NX00-3AE0 |
|
SIMATIC NET PB S7-5613
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1713-5CB00-3AE1 |
|
SIMATIC NET PB S7-5613
UPGRADE for EDITION 2006 and higher |
6GK1713-5CB00-3AE0 |
|
SIMATIC NET PB DP-5613
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1713-5DB00-3AE1 |
|
SIMATIC NET PB DP-5613
UPGRADE for EDITION 2006 and higher |
6GK1713-5DB00-3AE0 |
|
SIMATIC NET PB FMS-5613
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1713-5FB00-3AE1 |
|
SIMATIC NET PB FMS-5613
UPGRADE for EDITION 2006 and higher |
6GK1713-5FB00-3AE0 |
|
SIMATIC NET, S7-REDCONNECT
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1716-0HB00-3AE1 |
|
SIMATIC NET, S7-REDCONNECT
UPGRADE for EDITION 2006 and higher |
6GK1716-0HB00-3AE0 |
|
SIMATIC NET IE S7-1613
UPGRADE for V6.0, V6.1, V6.2 and EDITION 2005 |
6GK1716-1CB00-3AE1 |
|
SIMATIC NET IE TF-1613
UPGRADE for EDITION 2006 and higher |
6GK1716-1TB00-3AE0 |
Please note that the supply of DX OPC Server products has been discontinued effective October 01, 2008 (see entry ID 31507617) and are thus no longer available as new products. This also concerns upgrades and the Software Update Service.
3. SIMATIC NET Manual Collection CD Edition 09/2008 (Electronic user manuals)
|
Product |
Version/Edition |
Order No. |
|
SIMATIC NET Manual Collection |
09/2008 |
6GK1975-1AA00-3AA0 |
This CD can be ordered separately, but is also included in the scope of supply of the above software products. The CD is also included with a number of further SIMATIC NET products and in this way replaces the printed documentation for these products.
4. User interface and OPC Server
The standard user interface is the OPC interface to the OPC Server. The OPC Server is included in the scope of supply of the relevant software products. In this way the user obtains access via OPC as standard programming interface. The following OPC Server/ OPC interfaces are included in the relevant products:
4.1 PROFIBUS
|
Product |
Includes OPC Server / OPC Interface for ..... |
|
DP-5613 |
PROFIBUS-DP
S5-compatible communication (FDL) |
|
S7-5613 |
S7 communication |
|
FMS-5613 |
FMS communication |
|
CP5613/CP5614 and CP 5613 FO7CP 5614 FO with DP-Base software |
S5-compatible communication(FDL)
PROFIBUS-DP (master)
access to DP slave of the CP 5614 |
|
SOFTNET-S7 PROFIBUS |
S7 communication |
|
SOFTNET-DP |
PROFIBUS-DP
S5-compatible communication(FDL) |
|
SOFTNET-DP Slave |
PROFIBUS-DP (slave) |
4.2 INDUSTRIAL ETHERNET / PROFINET / SNMP / Data Exchange
|
Product |
Includes OPC Server / OPC Interface for ..... |
|
S7-1613
S7-Redconnect |
S7 communication
S5-compatible communication(SR) |
|
TF-1613 |
S5-compatible communication(SR) |
|
SOFTNET-S7 / -S7 Lean |
S7 communication
S5-compatible communication(SR) |
|
SOFTNET-PROFINET IO |
PROFINET IO communication |
|
PROFINET CBA OPC-Server |
PROFINET CBA |
|
SNMP OPC-Server |
SNMP access via OPC |
5. Installation – New features of Edition 2008 compared to predecessor versions
After you have inserted the CD ROM with the Software Edition 2008 or after you have called up Setup.exe you will get the option to install the following products or perform the following actions:
- Display readme
- Install SIMATIC NET software
- Display SIMATIC NET documents
- Abort
If predecessor versions of the products are available already, this will be checked and you will be asked for permission for the required uninstallation via a message box. The subsequent installation will upgrade any existing SIMATIC NET products to the current version of the relevant CD ROM. This will ensure a safe and consistent operational environment. Each of the products used requires an appropriate product license. Products without installed license key are in “Trial Mode“ and the lack of a license will be indicated during use. |