show the entry list
Download of the Private MIB Text Files (Management Information Base) V4.0 and SNMP OPC Profile Version 1.0 for SCALANCE W-700
Part number:

 

Description:

These downloads include the latest version of the Private MIB (Management Information Base) V4.0, as well as SNMP OPC Profile Version 1.0 and can be used for the following SCALANCE W-700 units.

 

Order no.’s concerned:

Product Name

Order No.

US Order No.

W786-1PRO

6GK5786-1BA60-2AA0

6GK5786-1BA60-2AB0

W786-1PRO

6GK5786-1AA60-2AA0

6GK5786-1AA60-2AB0

W786-1PRO

6GK5786-1BB60-2AA0

6GK5786-1BB60-2AB0

W786-1PRO

6GK5786-1AB60-2AA0

6GK5786-1AB60-2AB0

W786-2PRO

6GK5786-2BA60-2AA0

6GK5786-2BA60-2AB0

W786-2PRO

6GK5786-2AA60-2AA0

6GK5786-2AA60-2AB0

W786-2PRO

6GK5786-2BB60-2AA0

6GK5786-2BB60-2AB0

W786-2PRO

6GK5786-2AB60-2AA0

6GK5786-2AB60-2AB0

W786-2RR

6GK5786-2BA60-6AA0

6GK5786-2BA60-6AB0

W786-2RR

6GK5786-2AA60-6AA0

6GK5786-2AA60-6AB0

W786-3PRO

6GK5786-3AA60-2AA0

6GK5786-3BA60-2AB0

W786-3PRO

6GK5786-3AB60-2AA0

6GK5786-3AB60-2AB0

W784-1

6GK5784-1AA30-2AA0

6GK5784-1AA30-2AB0

W784-1RR

6GK5784-1AA30-6AA0

6GK5784-1AA30-6AB0

W744-1

6GK5744-1AA30-2AA0

6GK5744-1AA30-2AB0

W746-1

6GK5746-1AA30-4AA0

6GK5746-1AA30-4AB0

W747-1

6GK5747-1AA30-6AA0

6GK5747-1AA30-6AB0

W788-1PRO

6GK5788-1AA60-2AA0

6GK5788-1AA60-2AB0

W788-2PRO

6GK5788-2AA60-2AA0

6GK5788-2AA60-2AB0

W788-1RR

6GK5788-1AA60-6AA0

6GK5788-1AA60-6AB0

W788-2RR

6GK5788-2AA60-6AA0

6GK5788-2AA60-6AB0

W744-1PRO

6GK5744-1AA60-2AA0

6GK5744-1AA60-2AB0

W746-1PRO

6GK5746-1AA60-4AA0

6GK5746-1AA60-4AB0

W746-1PRO

6GK5746-1AA60-4BA0

--

W747-1RR

6GK5747-1AA60-6AA0

6GK5747-1AA60-6AB0

Download procedure:

When you dispatch the form below, a download button will be activated automatically with which you can download the free self-unpacking file "scalance_w700.exe". Double clicking this file will generate the file "SN_SCALANCE_W700_V40.MIB" and the file "Profil_SCALANCE_W700_V10.txt".

 

Here  ( 99 KB ) you can download the files.

 

#Ende#

 Entry ID:31483794   Date:2008-09-09 
I regard this article....as helpfulas not helpful                                 
related links
Private MIB (Management Informati ...
Download of the Text Files Privat ...
Declaration of Conformity, EC-Dec ...
Test Certificates, inspection cer ...
Radio Equipment Type Approval Cer ...