show the entry list
SIMATIC TDC Communication -- Configuring and programming communication -- Configuring the PROFIBUS interface
How can you clear communication error 69A1 with an EXM448, EXM448-1 or CP50M0 as slave on the PROFIBUS?
How do you read and write drive parameters via PROFIBUS DP with the SIMATIC TDC?
How can the SIMATIC TDC module CP50M1 as DP master read the input data of a DP slave that has been configured by another DP master (direct data exchange - DX)?
How can the SIMATIC TDC module CP50M1 be configured as a PROFIBUS DP slave?
How do you read and write drive parameters via PROFIBUS DP with the SIMATIC TDC?
Part number:

Instructions:
In order to be able to read and write drive parameters from and to a SIMATIC TDC configuration, you require an extensive configuration of approx. 30 standard CFC function blocks. Pay attention here to the correct interconnection and correct choice of order of processing.
The sample configuration attached helps SIMATIC TDC users to handle the drive parameters. The example consists of a Chart-In-Chart and can process exactly one parameter. If more than one parameter are to be handled, you can open the Chart-In-Chart and increase the number of parameters to be handled to suit your requirements.

Downloads
 
Content of the downloads Download
User Notes ( 667 KB )
Sample configuration ( 1318 KB )

 Entry ID:27206321   Date:2008-01-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour